×
Siemens Industry Online Support
Siemens AG
文档类型 软件下载 文档编号 109756318, 文档发布日期 2018年4月25日
(0)
评估

SINAMICS Support Packages for SINAMICS STARTER to operate medium-voltage converters GH150, GL150, GM150, SM120, SL150, SM150

  • 文档
  • 涉及产品
OSS note regarding SSP SINAMICS MV V4.8 SP2

Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:

 Registrierung notwendig  ReadMe_OSS.zip (21.0 KB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the following file SSP_SINAMICS_MV_V4_8_SP2.zip (in folder...\02_OSS_Information\Open_Source_Software.zip).

SSPs for updating existing installations of STARTER >=V4.5.1.x - or also SCOUT >=V5.1  (SSP installation in "SCOUT TIA" not possible. Observe the detailed description.)


STARTER
>=
V4.5.1

SCOUT
>=
V5.1

 Registrierung notwendig  SSP_SINAMICS_MV_V4_8_SP2HF1.zip (27,9 MB)

X

X

 Registrierung notwendig  ReadMe_OSS.zip (21.0 KB) 

X

SSP, SINAMICS MV V4.8 SP2

Here, as individual download, you will find the SINAMICS Support Package (SSP) SINAMICS MV V4.8.2 that matches STARTER >= V4.5.1 or SCOUT  >= V5.1

With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS MV series with firmware release V4.8.2 can be configured and commissioned using STARTER V4.5.1 or SCOUT V5.1

Procedure for installing the SSP:

  1. Download the attached ZIP file.
  2. Unzip the ZIP file to a shared target directory on your hard disk
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follows:
    \...\01_Readme\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important information on how to use the tool.

After installing SSP for STARTER V4.5.1 or SCOUT V5.1,  the following drive systems are also supported

  • SINAMICS MV V4.8.2
    • Specifically, these are as follows: GH150, GL150, GM150, SM120, SL150, SM150

Note regarding the online help for function release V4.8.2:

When installing SSP SINAMICS MV V4.8 SP2, the content of STARTER online help is not updated.
Updating this online help for V4.8.2 is possible by installing the help package for STARTER V4.5 SP1.

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
对统计的支持
用该功能可根据所需数量输出搜索结果的IDs (格式 .txt)

生成列表
复制URL
在新设计中显示此页面
mySupport Cockpit