×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109756570, Entry date: 04/26/2018
(7)
Rate

SIMATIC Virtualization as a Service - V3.3 Sales and Delivery Release

  • Entry
  • Associated product(s)
SIMATIC Virtualization as a Service version 3.3 has been released for sale and delivery effective immediately.

Important changes to the previous version:

 

  • Change of the SIVaaS product structure due to the new Microsoft Windows Server license model:

    Previously:

    Microsoft Windows Server standard license is installed on each virtual machine (VM), regardless of the physical hardware specification.

    Microsoft Windows 2012 standard license was bound to the article number of the VM.


    New:

    The Microsoft Windows Server 2016 license model depends on the physical hardware specification (number of cores in the server).




    This results in price changes in the SIVaaS system. For detailed information, please get in touch with your regional Siemens contact person.


  • Siemens' own SIMATIC Industrial thin clients are now also available as management consoles in various versions. Thin clients are delivered with VMware vSphere Web client software.

  • Virtual Storage Area Network (vSAN) host standard MLFBs (article numbers) are available effective immediately.

  • New virtual machines for PCS 7 V9.0 SP1.

  • New virtual machines for new versions of Route Control servers and client.

  • New virtual machines for the new Version of SIMIT V9.1.

  • New version of VMware V6.5 is available.

  • We can still deliver the discontinued Microsoft Windows Server 2012 R2 operating system on SIVaaS platform.

  • The virtualized system platform on an SIMATIC IPC will be available as of May 2018. The IPC Host is suitable for WinCC Classic applications as of version 7.

Standard hosts with new license model

MLFB

10Cx1P HP Host System

9LA1110-6SV00-1HB2

14Cx1P HP Host System

9LA1110-6SV00-1HC2

10Cx2P HP Host System

9LA1110-6SV00-1HE2

14Cx2P HP Host System

9LA1110-6SV00-1HF2

4Cx1P Siemens IPC Host System

Available as of May 2018

vSAN Hosts

MLFB

14Cx1P HP vSAN System

9LA1110-6SV00-1HL2

10Cx2P HP vSAN System

9LA1110-6SV00-1HM2

HPE 5130 24G switch

9LA1110-6SV00-1SW0

Service contracts for vSAN HOSTS

MLFB

2-year service contract for 14Cx1P vSAN Host

9LA1110-6SV00-1AL1

2-year service contract for 10Cx2P vSAN Host

9LA1110-6SV00-1AM1

5-year service contract for 14Cx1P vSAN Host

9LA1110-6SV00-1AL3

5-year service contract for 10Cx2P vSAN Host

9LA1110-6SV00-1AM3

2-year service contract for HPE 5130 24G Switch

9LA1110-6SV00-1SW1

5-year service contract for HPE 5130 24G Switch

9LA1110-6SV00-1SW3

New virtual machines

MLFB

VM with W2016 Server 64-bit

9LA1110-6SV05-0AA3

VM with PCS 7 V9.0 SP1 OS Servers

9LA1110-6SV05-1AB4

VM with PCS 7 V9.0 SP1 ES/OS Client

9LA1110-6SV05-1GB6

VM with PCS 7 V9.0 SP1 OS Client

9LA1110-6SV05-1HB4

VM with PCS 7 V9.0 SP1 BATCH Servers

9LA1110-6SV05-1LB4

VM with PCS 7 V9.0 SP1 BATCH Client / OS Client

9LA1110-6SV05-1JB4

VM with PCS 7 V9.0 SP1 Route Control Servers

9LA1110-6SV05-1MB4

VM with PCS 7 V9.0 SP1 Route Control Client

9LA1110-6SV05-1NB4

VM with SIMIT V9.1 Simulations Software

9LA1110-6SV05-0SM2

VM with SIMIT V9.1 Virtual Controller

9LA1110-6SV05-0SM3

New Siemens Industry Thin Clients

MLFB

SIMATIC IPC327E Basic Box PC

6AG4022-0AA21-1CA1

SIMATIC IPC377E Basic Panel PC – 15"

6AV7230-0DA20-1CA0

SIMATIC IPC377E Basic Panel PC – 19"

6AV7230-0EA20-1CA0

SIMATIC  ITC1500 V3 – Multitouch Screen 15"

6AV6646-1BA15-0AA0

SIMATIC  ITC1500 V3 – Multitouch Screen 19"

6AV6646-1BA18-0AA0

SIMATIC  ITC1500 V3 –  Multitouch Screen 22"

6AV6646-1BA22-0AA0

  

Click on the following link for more marketing information on SIMATIC Virtualization as a Service: https://www.siemens.com/global/en/home/products/services/industry/digital-industry-services/simatic-virtualization-as-a-service.html  

Our product support is available to registered users: https://support.industry.siemens.com/cs/de/en/ps/20178 


If you have any questions, please contact your regional sales representative via the global contact database           


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.