×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109756635, Entry date: 03/22/2018
(0)
Rate

Error message during compilation with LIBRARY PAC/3WL/3VA SIMATIC PCS7 SW+COL

  • Entry
  • Associated product(s)

Question:

Warum erscheint bei der Übersetzung des S7-Programms mit der LIBRARYeine Fehlermeldung in PCS 7 V9.0 mit / ohne SP1?

Why appears during compilation of PLC program with LIBRARY PAC/3WL/3VA SIMATIC PCS7 an error message


Answer:

During compilation of an S7 PLC program with LIBRARY PAC/3WL/3VA SIMATIC PCS7 SW + COL (3ZS2787-1CC30-0YG0) with a PROFINET communication interface in PCS 7 V9.0 with and without SP1 it comes the error message:

"Parameter Mccb3Va.DrvC800.BrkAvail is not interconnected with a data source (block output, global address)".

To resolve the problem you have to copy the attached files in the following path

...\SIEMENS\STEP7\S7DATA\driver\object

Then replace the existing files, compile again and continue as usual.

 Registrierung notwendig  PNDRVSWTSENTRON3VA.xml (1 KB)

 Registrierung notwendig  PNDRVSWTSENTRONPAC.xml (1 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.