×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109756716, Entry date: 03/26/2018
(1)
Rate

Industrial Thin Client Firmware V2.0.2 Service Pack 6 (V2.0.2.6)

  • Entry
  • Associated product(s)
This update contains improvements to existing components. It can be installed and used on all Industrial Thin Clients ITC1200, ITC1500, ITC1900, ITC2200. Service Pack 6 also introduced NLA support for RDP and a Spanish keyboard layout for the on-screen keyboard for local configuration.

Update information

You can find detailed information on ITC and the update under entry 109477666

This version includes Service Pack 3 (V2.0.2.6)

Service Pack 6 introduced NLA support for RDP and a Spanish keyboard layout for the on-screen keyboard for local configuration.
 

Update instructions

The update can be performed in 2 ways:
1. Directly on the Industrial Thin Client using a USB stick
2. From a PC using remote configuration

Important
In both cases, the factory settings of the ITC are restored after the update and all other settings are lost during the update.

It is recommended that you back up your ITC configuration before the update.
If you use the RCC to back up the configuration, ensure that you use the appropriate RCC version. Back up the configuration files of a version <= V2.0.1.1 using RCC with a version <= V2.0.1.

Using RCC (Remote Configuration Center) >= V2.0.2, it is possible to back up the configuration files with a FW version >= V2.0.2.
To restore the configuration files, RCC version V2.0.2 can be used after the update of the firmware to V2.0.2.

Note:
If the power supply or the connection to the device containing the firmware is interrupted during the update process, the device may no longer be functional. Ensure that the power supply to the device and the connection are maintained during the entire update process. Ensure that all applications running on the device are closed. Before you update the firmware, back up the ITC configuration file if needed. Procedure
Installation directly on the device using a USB stick.

Procedure:

1. Transfer the update file "update_v2_0_2_x.upd" to a USB stick
2. Connect this USB stick to one of the two rear USB ports of the ITC
3. Open the "Configuration" menu from the taskbar on the ITC
4. Log on as administrator
5. Under "System", select "Update" in the Device configuration/Firmware version section
6. Select the update file "update_v2_0_2_x.upd" on the USB stick and start the update with "OK". 

To determine whether the selected file is suitable for the Industrial Thin Client, the system checks the following conditions:
• The selected file is an update file.
• The selected update file is newer than the version installed on the Thin Client.
• The selected update file is suitable for the Industrial Thin Client at hand.

If all the conditions are met, the selected update file is executed on the device. The progress of the update is displayed on the screen.
After a successful update, the device is rebooted and the setup wizard appears.

Installation via the Remote Configuration Center (as of V2.0)

The Remote Configuration Center (RCC) enables you to update the firmware of a device or multiple devices from a PC.
For a firmware update to versions as of  V2.0.2, you also need RCC with a version as of >= V2.0.2. Otherwise, the firmware of the device will not be updated.
The RCC is included in the SIMATIC ITC product package and can also be downloaded (link below).

Procedure for updating a device

  1. Back up the configuration file of the ITC device. For firmware versions <= V2.0.1, use RCC V2.0.1 or back up the file directly in the configuration center of the device:
  2. Under "System", select "Update" in the Device configuration/Firmware version section
  3. Select the update file "update_v2_0_2_x.upd" from the preset directory and start the update with "OK"

Procedure for updating multiple devices:

  1. Open the RCC and select all relevant ITCs
  2. Select the "Update Firmware" button
  3. Select the update file "update_v2_0_2_x.upd" from the preset directory and start the update with "OK"

To establish whether the selected file is suitable for the Industrial Thin Client, the system checks the following conditions:

  • The selected file is an update file.
  • The selected update file is newer than the version installed on the Industrial Thin Client.
  • The selected update file is suitable for the Industrial Thin Client at hand.

If all the conditions are met, the selected update file is executed on the device. The progress of the update is displayed on the screen. After a successful update, the device is rebooted and the setup wizard appears.

Additional information about updating firmware using the Remote Configuration Center:

  • You can find an overview of supported operating systems in the manual.
  • Parallel installation of RCC V2.0.2 with earlier versions (<V 2.0.2) is not possible. These versions are uninstalled automatically. V1.x versions remain installed.
  • Since the configuration data is encoded with the new version of RCC, note the following:
  • Using RCC V2.0.2, all devices with firmware V2.0.x can be updated to version V2.0.2.

Note the following when backing up the configuration file of the device.

  • The configuration file can be backed up beforehand from the device in the configuration center of the device or using RCC V2.0.1.
  • The backed up configuration file can be transferred to the device without problem after upgrading the device to FW V2.0.2 using RCC V2.0.2.

Third-party software – license conditions and copyright notes

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the Readme_OSS.pdf file.

Special note for resellers

The information and the license terms in the Readme_OSS.pdf file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  ReadMe_OSS.htm (13,9 MB)



You can find the update of the Open Source DVD accompanying the "Industrial Thin Client" products, including the corresponding source code, here:
 Download unterliegt Exportcontrolle  OpenSourceSoftware.zip (564.9 MB)
(This software is subject to export restrictions, download for registered users only)

Download of software/firmware

Download ITC Firmware V2.0.2.x
 Download unterliegt Exportcontrolle  update_v2_0_2_6.zip (171.5 MB)
(This software is subject to export restrictions, download for registered users only)

Download ITC Remote Configuration Center V2.0.2.x (RCC)
 Download unterliegt Exportcontrolle  ThinClient_V2.0.2_RCC.zip (250.4 MB)
(This software is subject to export restrictions, download for registered users only)

Download Complete Package ITC_V2.0.2.x
 Download unterliegt Exportcontrolle  ThinClient_V2.0.2_FW_RCC.zip (421.9 MB)
(This software is subject to export restrictions, download for registered users only)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.