SINAMICS firmware version 4.7 SP10 HF6 for SINAMICS G120 (CU240B/E-2, CU250S-2), G120P (CU230P-2), G120C, G120D (CU240D-2, CU250D-2), G110M and SIMATIC ET200pro FC-2 products
-
Entry
-
Associated product(s)
Content of the SINAMICS G120 multicard V4.7 SP10 HF6 | ||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
In this entry you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 SP10 HF6. The associated sales information is available under 109755811.
The installed firmware version can be read out at the SINAMICS G module using parameter r0018 (internal version) or r0964 (complete device identification). From V4.7 SP10, an parameter r7844[1] is available to display the firmware version. The value contained in it, e.g. "04071508", corresponds to firmware version V4.7 SP10 HF6. Note
An overview of the available firmware releases for SINAMICS G is provided under: 67364620. |
Third-party software – license conditions and copyright notes |
---|
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file READ_OSS.HTM file. Special note for resellers The notes and the license conditions contained in the READ_OSS.HTM file must be passed on to the purchaser in order to avoid the reseller and purchaser from violating the licensing conditions. Availability of the source code Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information either directly on the product itself or with the product (e.g. on a mass storage medium, DVD). Should this not be possible due to technical reasons, Siemens will send you this OSS Source Code against payment of the handling expenses. Please contact the address specified at the end of this section regarding this matter. Siemens AG |
Current list of general conditions of the SINAMICS G120 for firmware V4.7 SP10 HF6 |
---|
![]() |
Functional restrictions which have been corrected for the SINAMICS G120 firmware V4.7 SP10 HF6 |
---|
![]() ![]() |
Provision of the SINAMICS G120 multicard V4.7 SP10 HF6 |
---|
The content of the SINAMICS G120 multicard described above can be downloaded here:
Note: Alternatively, the SINAMICS G120 multicard V4.7 SP10 HF6 (SD card) can be ordered using the following article number Instructions for upgrading the SINAMICS G120 firmware: When upgrading, please refer to the instructions given in the "Firmware upgrade" chapter in the operating instructions of the particular Control Unit. As an example, you can find the firmware upgrade/downgrade instructions for the SINAMICS CU240E-2 here:
Note: |
List of faults and alarms |
---|
List of faults and alarms for SINAMICS CU230P-2 |
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120P in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS G120P product is concerned, no additional support can be provided here.
|
List of faults and alarms for SINAMICS CU240B-2 and CU240E-2 |
---|
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the SINAMICS G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS G120 product is concerned, no additional support can be provided here.
|
List of faults and alarms for the SINAMICS CU240D-2 and CU250D-2 |
---|
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120D in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS G120D product is concerned, no additional support can be provided here.
|
List of faults and alarms for SINAMICS CU250S-2 |
---|
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS G120 product is concerned, no additional support can be provided here.
|
List of faults and alarms of the SINAMICS G120C |
---|
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the SINAMICS G120C in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS G120C product is concerned, no additional support can be provided here.
|
List of faults and alarms of the SINAMICS G110M |
---|
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the SINAMICS G110M in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS G110M product is concerned, no additional support can be provided here.
|
List of faults and alarms of the SINAMICS ET200pro FC-2 |
---|
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the SINAMICS ET200pro FC-2 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the SINAMICS ET200pro FC-2 product is concerned, no additional support can be provided here.
|
GSD files for project integration into the PROFIBUS configuring tool |
---|
PROFIBUS GSD files can be downloaded in the following entries: |
GSDML files for integrating projects into the PROFINET configuring tool |
---|
PROFINET GSDML files can be downloaded in the following entries: |
EDS files for integrating projects into the CANopen configuring tool |
---|
The EDS files for integrating projects into the CANopen configuring tools can be downloaded under 48351511. |
STARTER |
---|
Within the scope of SINAMICS firmware version V4.7 SP10 HF6, STARTER V5.1 SP1 (see 109753725) must be used with the SINAMICS Support Package (SSP). SSP is available under 109477753 .
As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with STARTER V4.4 SP1 and SINAMICS G firmware V4.7 SP3. For additional information, refer to 109480663. |
Startdrive |
---|
Within the scope of SINAMICS firmware version V4.7 SP10 HF6, Startdrive V15 (see 109752254) including the Hardware Support Package (HSP) V4.7 SP10 should be used (see 109754382). It is also possible to use Startdrive V14 SP1 (see 109746259) with the corresponding Hardware Support Package (HSP) V4.7 SP10 (see 68034568). As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with Startdrive V13 SP1 and SINAMICS G firmware V4.7 SP3. Additional information should be taken from the Entry 109480663. |
IOP-2/BOP-2 |
---|
The HMI device IOP-2 (Article No.: 6SL3255-0AA00-4JA2) with firmware V2.3 supports the expanded functions of the SINAMICS G firmware V4.7 SP10 HF6. A complete list of the expanded functionality for IOP-2 V2.2 can be taken from the release for sale and delivery 109762019. In order to upgrade an existing IOP-2, the entry also includes an IOP-2 firmware download. The BOP-2 operator panel (Article No.: 6SL3255-0AA00-4CA1) is automatically updated when using firmware V4.7 SP10 HF6. As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with SINAMICS G firmware V4.7 SP3. For additional information on this subject please refer to entry 109480663. |
- German
Entry belongs to product tree folder(s):
- Drive Technology Converters Low voltage converters Decentralized Frequency Converters SINAMICS G110M Motor-Integrated Frequency Converters
- Drive Technology Converters Low voltage converters Industry-specific frequency converters SINAMICS G120P for Pumps, Fans and Compressors SINAMICS G120P Built-In and Wall-Mounting Units
- Drive Technology Converters Low voltage converters Industry-specific frequency converters SINAMICS G120P for Pumps, Fans and Compressors SINAMICS G120P Cabinet
- Drive Technology Converters Low voltage converters Decentralized Frequency Converters SINAMICS G120D Distributed Converters
- Drive Technology Converters Low voltage converters Standard Performance Frequency Converter SINAMICS G120C Built-In Units
- Drive Technology Converters Low voltage converters Standard Performance Frequency Converter SINAMICS G120 Built-In Units Control Units
- Drive Technology Converters Low voltage converters Standard Performance Frequency Converter SINAMICS G120 Built-In Units Power Modules
- Drive Technology Converters Low voltage converters Decentralized Frequency Converters Converters for SIMATIC ET 200pro Distributed IO
- Safety systems - Safety Integrated Safety Technology for Factory Automation Drive technology SINAMICS G120 Built-in Units
- Safety systems - Safety Integrated Safety Technology for Factory Automation Drive technology SINAMICS G120D Distributed Frequency Inverters
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry