×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109756879, Entry date: 07/20/2018
(2)
Rate

Software SIMOCODE pro PCS 7 Library V9.0 + SP1

  • Entry
  • Associated product(s)
The software SIMOCODE pro PCS 7 Library V9.0 + SP1 is now available for download. With this download, an existing installation of SIMOCODE pro PCS 7 V9.0 Library can be updated to V9.0 + SP1.

What is new in V9.0 + SP1?

New Features

  1. Support for SIMOCODE pro V FW V4.0 and SIMOCODE pro V PN FW V2.0 along with its new features.   
  2. Support for UM+ (2nd Generation current/voltage) range of modules.
  3. Detection of UM+ module, Digital Module1 and 2 – Bistable, Digital Module1 and 2 – Monostable, Earth-fault module 2 (EM+) at DevFunc Output in MMOprtn block.
  4. New device diagnostic events at Operation faceplate.
    • Internal Earth Fault
    • BU FW Update Activ
    • Module FW Update Active.
  5. New error type message related to FW Update and HW Fault is now available at Logbook faceplate with a timestamp 
  6. Frequency and Average Current Detection in Measurement faceplate.
  7. Consumed Energy at Statistical faceplate is displayed now as float values with 2 decimals.
  8. Higher precision Float values display with 2 decimal for the following parameters at Measurement faceplate along with Cyclic reading.
    • Frequency
    • Current I_max
    • Current I_Avg
    • Current I_L1
    • Current I_L2
    • Current I_L3
    • Active Power
    • Apparent Power
    • Voltage UL1
    • Voltage UL2
    • Voltage UL3
    • Cos-Phi
  9. Reading Configuration Data via mini faceplate “Right click” at SIMOCODE pro Block icon.
  10. Resetting the error via mini faceplate by “Right click” on Error Symbol in SIMOCODE pro Block Icon.
  11. When one or more messages are suppressed a new Alarm Suppression indication is added at the Faceplate overview toolbar of SIMOCODE pro Blocks.
  12. Disabling of unsupported Voltage measurement view at MMMeas faceplate when SIMOCODE pro C/S is configured.
  13. Feature Bit 9 at FbSwtMMS block has been updated with value 1 at the control function templates. This has been done to support the enhanced driver generation handling at CFC V9.0 + SP1 + Upd2.
    The Feature Bit 9 at the FbSwtMMS channel block determines the library to be used for generating module driver during compilation. This allows simultaneous module driver generation of an add-on library in addition to the Basis Library for different HW Config devices.

 Bug Fixes

  1. In Logbook faceplate when PROFIBUS device is configured Date column is additionally displayed, which is applicable only for PROFINET devices. This issue has been solved now.
  2. When the faceplate is open and if the OS permission is disabled Read data button is still enabled, this behavior has been corrected at MMOprtn and MMLog faceplates.
  3. When PORT diagnostic is activated and one end of the ring network is removed from an MRP configuration with SCALANCE in this case device failure will be reported
  4. Warnings during driver generation for PROFINET devices when SIMOCODE pro Library is used in parallel with other Libraries (i.e. DRIVE-ES, SENTRON...).

    E.g. When SCALANCE-X216 with BASIS Library is configured in conjunction with SIMOCODE pro PCS 7 Library in the project, driver generation gives the following warning for the SCALANCE device “W: SCALANCE-X216 (6GK5 216-0BA00-2AA3) is not supported”. In this case SCALANCE-X216 device is hindered by the SIMOCODE pro Library files and corresponding diagnostic blocks are not created. This issue has been resolved in SIMOCODE pro PCS 7 Library V9.0 SP1.


Installation notes:

Please observe the description of new features and alterations, the installation and application notes available in the file MMReadme.zip which can be downloaded here:

 Registrierung notwendig  MMReadme.zip (61,3 KB)

SIMOCODE pro PCS 7 Library V9.0 + SP1 is offered in the form of the download file „SIMOCODE_pro_PCS7_Library_V9.0_SP1.exe“. Please first download this file and then execute it. Afterwards, the file will be extracted and you can execute the setup. Please exit all STEP 7 applications prior to starting the installation.


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS_Global.htm file.

Special information for resellers

The information and the license terms in the Readme_OSS_Global.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Readme_OSS.zip (42,9 KB)


Download

 Registrierung notwendig  SIMOCODE_pro_PCS7_Library_V9.0_SP1.exe (280,2 MB)

SHA-256 checksum:   Registrierung notwendig  Code_SIMOCODE_pro_PCS7_Library_V9.0_SP1.txt (1 KB)
Information about SHA-256:  109483101 



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.