×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109756885, Entry date: 05/25/2018
(3)
Rate

OPC UA methods for the SIMATIC S7-1500 OPC UA server

  • Entry
  • Associated product(s)
As of firmware version V2.5 and TIA Portal V15, the SIMATIC S7-1500 control system also offers OPC UA methods for the clients via its integrated OPC UA server.

For standardized, communication of an S7 control system that applies to all platforms and manufacturers, Siemens offers you the communication protocol OPC UA.

As of firmware version V2.5 and TIA Portal V15, the SIMATIC S7-1500 control system can also offer OPC UA methods for the clients via its integrated OPC UA server. With this addition to the functions, you not only have the option of reading or writing OPC UA variables of the control system, you can now also start complex functional sequences via OPC UA. This enables almost complete M2M communication via OPC UA, for the networking of plants or for the control of plants from an ERP / MES level.

In this application example, we explain how to program an S7 function block so that it can be called as an OPC UA method on the server of an S7-1500.


 

Documentation and example project
  Documentation (1,1 MB)
 Registrierung notwendig  Project for STEP 7 V15 (1,1 MB)
 Registrierung notwendig  XML status codes for TIA Portal import (7,3 KB)
 

Additional keywords
Methoden, Methode,

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit