×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109756900, Entry date: 05/16/2018
(0)
Rate

Why can you not compile the Simulink model with SIMATIC Target 1500S V1.0 (Upd1)?

  • Entry
  • Associated product(s)
Compilation of the Simulink model with SIMATIC Target V1.0 (Upd1) fails if you have installed version V1.0 (Upd1) after installation of V2.0.

Description
To clear this behavior you have to remove the Target 1500S V2.0 as system target file from the corresponding MATLAB version and then re-insert it.

You have two options for this:

  • Uninstall the Target 1500S V2.0 software (highest release version) and then re-install.
  • From the installation path of Target 1500S V2.0, via the Windows Command Prompt you run the "target_integrator.exe" tool.

procedure for running the "target_integrator.exe" tool

  1. Close all the open programs including MATLAB/Simulink.
  2. Start the Windows Command Prompt (cmd.exe) as Administrator.
  3. Using the command "cd" and the relevant path you switch to the folder '\bin' in the installation directory of Target 1500S V2.0.


    Fig. 1
     
  4. Execute the command "target_integrator –h" to display the Help for using the tool.


    Fig. 2
     
  5. Execute the command "target_integrator uninstall –a" to remove Target V2.0 from all the compatible MATLAB versions.
    Alternative: Execute the command "target_integrator uninstall - path <path_to_matlab_exe>" to remove Target V2.0 from a specific MATLAB version.


    Fig. 3
     
  6. Execute the command "target_integrator install –a" to re-insert Target V2.0 in all the compatible MATLAB versions.
    Alternative: Execute the command "target_integrator install - path <path_to_matlab_exe>" to re-insert Target V2.0 in a specific MATLAB version.


    Fig. 4

Additional Keywords
Build Model, Code generation, Generate model, Fail, Error

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.