×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109756912, Entry date: 07/28/2020
(0)
Rate

Description of the SIMOCODE pro V EIP firmware update

  • Entry
  • Associated product(s)
Description of the firmware update for the SIMOCODE pro V EIP motor management system

Description:
During operation it may be necessary to update the firmware (e.g. to extend the available functions).
Update the SIMOCODE pro V EIP firmware for the basic unit with the aid of firmware files. The parameterization of the device is retained after the firmware has been updated.

Requirements:

  • The supply voltage to the basic unit must be present and the network connection must not be interrupted at the start or during the firmware update.
  • A firmware update is only possible if
    • The motor is in the "off" state and there is no motor current
    • The control station is in "Local manual" status
    • The device is not protected by a password

Options for the firmware update

A firmware update can be performed via PROFINET IO with STEP 7 or SIMOCODE ES (TIA Portal).

Installation of the firmware update


Procedure via SIMOCODE ES (TIA Portal)

Proceed as follows to perform an online firmware update with SIMOCODE ES:

  1. Select the module in the device view.
  2. Select the "Online & diagnostics" command from the shortcut menu.
  3. Select the "Firmware update" group from the "Functions" folder.
  4. Click the "Browse" button to select the path to the firmware update files in the "Firmware update" area.
  5. Select the firmware file "3UF7 013-1AX00-0 V1.1.3.upd" from the folder in which the download file was earlier unpacked. The table in the firmware update area lists the modules under "Suitable for modules" for which an update is possible with the selected firmware file.
  6. Click the "Run update" button. If the module can interpret the selected file, the file is downloaded to the module.

Updating the firmware:

The "Run firmware after update" check box is always selected.
When the loading process is complete, the CPU adopts the firmware, and then operates with this new firmware.

Note:

If a firmware update is interrupted, the device cannot be used for production purposes until the update has been fully completed. In this case, the BUS and GEN FAULT LED indicators flash alternately and the DEVICE LED lights red. Restart the firmware update after an interruption.

Behavior during the firmware update:

Note the following behavior during the firmware update:

The BUS and GEN FAULT LED indicators flash alternately, and the DEVICE LED lights red. 

Behavior after the firmware update:

After the firmware update, check the firmware version of the basic unit that has had the firmware updated.

Reference:

Further information on the procedure is to be found in the SIMOCODE ES online help.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Read_Me_OSS_EIP_V1.1.3.html file.

Special information for resellers

The information and the license terms in the Read_Me_OSS_EIP_V1.1.3.html file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Read_Me_OSS_EIP_V1.1.3.html (592,0 KB) 

Firmware Update for SIMOCODE pro V EIP

Article no.Release /
FW Version
Update with ....  
3UF7013-1AB00-0
3UF7
013-1AU00-0


 

*E01* / V1.0.0
*E01* / V1.0.1
*E02* / V1.0.1 /
V1.0.2
*E03* V1.0.2
*E04* / V1.1.1 / V1.1.2
*E05* / V1.1.2
 
 Update V1.1.3  Description (see below)

For SIMOCODE ES TIA-Portal (as from  V15 and higher)

 Registrierung notwendig  3UF7_013-1AX00-0_V1.1.3.zip (4,0 MB)

SHA-256 checksum:  Registrierung notwendig  Code_3UF7_013-1AX00-0_V1.1.3.txt (1 KB)

Information about SHA-256: 109483101

*E01* / V1.0.0 / V1.0.1
*E02* / V1.0.1 / V1.0.2
*E03* / V1.0.2
 *E04* / V1.1.1
 
Update V1.1.2  Description (see below)


*E01* / V1.0.0 / V1.0.1
*E02* / V1.0.1 / V1.0.2

Update V1.1.1  Description (see below)

*E01* / V1.0.0 / V1.0.1
*E02* / V1.0.1 
Update V1.0.2 Description (see below)
 *E01* / V1.0.0Update V1.0.1 Description (see below)


Update V1.1.3
(contains also V1.0.2, V1.0.1, V1.1.1 and V1.1.2)

  • Web server: harmonization of displayed terms with the engineering software (language setting: English)
    Previously: General fault                     
    New: Group fault
    Previously: General warning               
    New: Group warning
    Previously: Test shutdown                  
    New: Test trip
    Previously: Thermal memory               
    New: Thermal motor model

  • Webserver: Device name assigned by SIMOCODE ES software is now being displayed in a more human-readable format

  • General improvements in terms of stability and security

  • Devices which have been updated to FW V1.1.3 cannot be downgraded to previous FW versions.

  • FW V1.1.3 also contains the function “dry running protection “.The use of this function necessarily requires basic units which are marked with *E04* or higher and “PTB 18 ATEX 5003 X".



Update V1.1.2
(contains also V1.0.2, V1.0.1 and V1.1.1)

  • Optimized test procedure of the thermistor inputs T1 and T2 during start-up phase
  • Devices which have been updated to FW V1.1.2 cannot be downgraded to previous FW versions.
  • FW V1.1.2 also contains the function “dry running protection “.The use of this function necessarily requires basic units which are marked with *E04* or higher and “PTB 18 ATEX 5003 X".
  • EDS file: 109741009


Update V1.1.1
(contains also V1.0.2 and V1.0.1)

  • STEP 7 V15.1 / SIMOCODE ES V15.1 with HSP 0295 SIMOCODE pro EIP / pro V required for parameterization

  • Web server with support for secured https connection including the function for enabling the control of the motor feeder when logged in with username and password.

  • Support of theEtherNet/IP feature Address Collision Detection (ACD)
  • Devices which have been updated to FW V1.1.1 cannot be downgraded to previous FW versions.
  • FW V1.1.1 also contains the function “dry running protection “. Because of the missing ATEX labeling, basic units which have been updated to FW V1.1.1 are not permitted to be used in combination with the current/voltage measuring modules for dry running protection of centrifugal pumps in Ex-zones (3UF7 12*). The use of this function necessarily requires basic units which are marked “PTB 18 ATEX 5003 X".
  • The thermistor inputs T1 and T2 must not be short-circuited during the start-up phase of the device.
  • EDS file: 109741009


Update V1.0.2
(contains also V1.0.1)

  • Update of the web server
  • Optimizations and stability improvements
  • EDS file: 109741009

Update V1.0.1

  • Optimization for SIMOCODE pro V EIP parameterizations which use more than 35 logic modules.
  • EDS file: 109741009
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.