×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109757079, Entry date: 04/26/2018
(3)
Rate

SSP SINAMICS G120 V4.7 SP10

  • Entry
  • Associated product(s)
SSP for updating existing STARTER or also SCOUT installations

Latest SINAMICS MICROMASTER STARTER

You can download the latest version of STARTER via: 26233208 


OSS note on SSP SINAMICS G120 V4.7 SP10
Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
 Registrierung notwendig  ReadMe_OSS.zip (287,9 KB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.zip file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability of OSS source code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source code and further information for these components. You can find this information in the file SSP_SINAMICS_G120_V4_7_SP10.zip (in the folder ...\02_OSS_Information\Open_Source_Software.zip).


SSP SINAMICS G120 V4.7 SP10

SSPs for updating existing STARTER or also SCOUT installations (observe detailed description)

SSP installation in "SCOUT TIA" is not possible!

can be installedintegrated

SSP, SINAMICS G120 V4.7 SP10
 Registrierung notwendig  SSP_SINAMICS_G120_V4_7_SP10.zip (19,7 MB)

SHA-512 checksum:
 Registrierung notwendig  sha512zip.txt (1 KB) 

Information about SHA-512: 109483101

STARTER
as of V5.1 SP1

SCOUT
as of V5.2 SP1 

STARTER
> V5.1 SP1 HF2

SCOUT
> V5.2 SP1


The associated online help (optional) can be found here: 109757069 

 


With this SINAMICS Support Package, SINAMICS G120/G120C/G120P/G120D drives with firmware version V4.7 SP9 can be configured and commissioned using STARTER or SCOUT.

Procedure for installing the SSP:

  1. Download the attached ZIP file.
  2. Unpack the ZIP file into a shared target directory on your hard disk. Please ensure that there are no spaces in the entire path name of this target directory.
  3. After unpacking, the shared directory must appear as follows:
    \...\01_Readme\
    \...\02_OSS_Information\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important information on how to use the tool.



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.