×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109757191, Entry date: 04/20/2018
(1)
Rate

SINAMICS S120 converter built-in devices, chassis format: System components, line-side power components

  • Entry
  • Associated product(s)
EMC filters for Category C2 according to EN61800-3

We would like to take this opportunity and inform you about an important correction relating to line filters for Chassis format devices.

The subsequently listed EMC filters have been developed and tested in accordance with EN61800-3.
However, this EMC standard is not applicable for the US market.
This is also the reason that these filters do not have UL certification.

Components involved:

6SL3000-0BE32-5AA0

6SL3000-0BE34-4AA0

6SL3000-0BE36-0AA0

6SL3000-0BE34-4AA0

6SL3000-0BE36-0AA0

6SL3000-0BE41-2AA0

6SL3000-0BE41-6AA0

6SL3000-0BG34-4AA0

6SL3000-0BG36-0AA0

6SL3000-0BG41-2AA0

6SL3000-0BG41-6AA0        

6SL3000-0BE35-0AA0

6SL3760-0MB00-0AA0

6SL3760-0MC00-0AA0

6SL3760-0ME00-0AA0

6SL3760-0MN00-0AA0

6SL3760-0MG00-0AA0

6SL3000-0BE33-1AA0

6SL3000-0BE35-0AA0

6SL3760-0MB00-0AA0

6SL3760-0MC00-0AA0

6SL3760-0ME00-0AA0

6SL3760-0MN00-0AA0

6SL3760-0MG00-0AA0      

The data for these filters in Catalog D21.3 (from Page 3/128) or D21.4 (from Page 7/197) were listed in such a way that could result in an incorrect interpretation regarding UL approval (which the filters do NOT have).

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.