×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109757452, Entry date: 05/18/2018
(0)
Rate

SITRANS/SIPART device library for SIMIT Simulation Platform

  • Entry
  • Associated product(s)
We provide you with a library of device-specific simulation blocks from the SITRANS and SIPART device family. The simulation models simulate the behavior of the corresponding actuators and sensors in their most important properties, making them ideal for virtual commissioning of process plants.

SIMIT Simulation Platform contains several standard components, such as drives and valves, for simulating devices and measuring points. This standard functionality is not sufficient for the simulation for every device installed in the system since the behavior of field devices can have a decisive influence on the behavior of the overall system. Modern field devices offer a multitude of functions and parameters that are only very inconvenient to simulate or cannot to be simulated with the standard SIMIT tools.

Specific device models have the requirement to exchange measured or controlled values and status signals with the PCS 7 driver blocks. The dynamic device behavior is simulated in SIMIT. In this application example, you can download a library of specific simulation models of the SITRANS and SIPART device family.



The device-specific simulation models offer you the following advantages:

  • Simulation of product-specific functions based on detailed device models
  • Increasing the accuracy and thus the benefit of the system model
  • Allows the determination of the optimal parameters of the field devices
  • Virtual commissioning of the devices in the context of plant simulation
  • Training of personnel in operator training systems (OTS) that realistically map the process behavior of the plant

The library includes the simulation models of the following devices:

  • SITRANS FC430, F M MAG 5000/6000, FX330, FUS060
  • SITRANS P DS III, P300, P310, P410, P500
  • SITRANS LR250, LR560, Probe LU, LUT400
  • SITRANS TH300, TH400
  • SIPART PS 2


Validation

The application example is valid for SIMIT SP V9.1.

Download
  Documentation (3,8 MB)
 Registrierung notwendig  SIMIT demo project (28,3 MB)
 Registrierung notwendig  SIMIT device library (1,6 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.