×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 109757654, Entry date: 05/14/2018
(0)
Rate

Sales and delivery release for SinuTrain for SINUMERIK Operate V4.8

  • Entry
  • Associated product(s)
The control-identical NC programming station SinuTrain for SINUMERIK Operate Version 4.8 has been released for sale and delivery.



SinuTrain for SINUMERIK Operate V4.8

The SinuTrain offline programming station brings SINUMERIK Operate to your PC, including an animated machine control panel, in a realistic way and facilitates the transfer of know-how from the training environment to the workplace. This powerful tool allows users to program offline at their PC, based on the DIN 66025 programming language and the ShopMill and ShopTurn options and SINUMERIK 828D and 840D sl language commands under realistic conditions. NC programs that have been generated can then be directly transferred to the CNC. With SINUMERIK Operate and its original SINUMERIK CNC kernel, all operations and programming steps as well as processing of CNC programs can be used without restrictions.

SinuTrain for SINUMERIK Operate V4.8 is based on SINUMERIK 840D sl CNC software 4.8 SP2.

A free basic version is available on our website CNC4you:
www.siemens.com/sinutrain-downloads

New features

  • SINUMERIK V4.8 SP2
  • Automation License Manager V6.0 HF1

  • Windows 10 release (as well as Windows 8.1 and Windows 7)

  • Integration of several SINUMERIK CNC software packages in one user interface

  • Display resolutions have been expanded, including 16:9

  • SinuTrain workbench with new functions:

    • Operation via menu bar and icons

    • All user machines are displayed as tiles, which can be arranged by dragging & dropping

    • Information tile to display all the important attributes of the selected machine

    • Assignment of user image files

    • Generation and management of user templates, including marking with own logo (not for SinuTrain Basic)

    • Multi-window mode: "Machine control panel" and "Operator panel" subwindows can be undocked in the machine simulation

  • Basic version (without valid license)

  • Integration of SINUMERIK Integrate Run MyScreens

  • Transfer of OEM-specific tool management

Creating a program

CNC programs that are created with SinuTrain can be used on real machines equipped with SINUMERIK 840D sl as well as SINUMERIK 828D. However, this is only possible if SinuTrain has been adapted to the SINUMERIK configuration of the machine. This can either be done by the user via the SinuTrain "Importing setup archive" option or by a Siemens expert whose services you can order (6FC5088-4AA22-4AB1).
Boundary conditions and compatibilities according to SINUMERIK CNC software and SINUMERIK 840D sl with respect to SINUMERIK 828D should be observed.

The following components have been released for delivery

in Germany and Austria

In countries where the product is distributed by Siemens Industry Software (currently Germany and Austria), the following article numbers apply:

Description

Single license (1)

Multi-station/classroom license (18)

SinuTrain

MCS40501

MCS40572

Import setup archive option

MCS40541

-

Delivery without software on data storage medium; customers will receive a download link to the GTAC download server.

Sales outside the abovementioned regions/countries

Description

Single license (1)

Multi-station/classroom license (18)

SinuTrain Basic

6FC5870-0YC45-0YA0

-

SinuTrain

6FC5870-4YC45-0YA0

6FC5870-8YC45-0YA0

SinuTrain upgrade *1)

6FC5870-4YC45-0YC0

6FC5870-8YC45-0YC0

Import setup archive option

6FC5870-0CC45-0YA0

-

SinuTrain notebook *2)

6FC5870-0YC45-0YT0

-

Delivery without software on data storage medium; to obtain the relevant data storage medium, the accompanying DVD can be ordered --> SinuTrain Basic 6FC5870-0YC45-0YA0.

*1) Not available in Germany, Austria: With the upgrade license, you can upgrade an existing SinuTrain Complete, SinuTrain ShopTurn or SinuTrain ShopMill to SinuTrain for SINUMERIK Operate V4.8. Prerequisite for the upgrade license is an existing, valid license key for the running period of SinuTrain versions 6.3, 7.3, 7.5, 2.6, 4.4, 4.5 or 4.7. This excludes SinuTrain Trial/Promotion and SinuTrain BASIC.

*2) Only available as a pack of 20

Contact

For additional information, please contact yourSiemens representative.

System requirements

Hardware

  • Processor: 2 GHz
  • RAM: 4 GB free storage space
  • Hard disk:

    • 3.3 GB for complete installation with all languages

    • 1.2 GB for minimal installation (in English)

  • Graphics: Minimum resolution 800*600 pixels

  • DirectX 9 or higher with WDDM 1.0 driver

  • Mouse, keyboard

Operating system

  • Windows 7 SP1 (32-bit and 64-bit; Starter, Web edition and Embedded are not supported)
  • Windows 8.1 (32-bit and 64-bit; RT edition is not supported)
  • Windows 10 (64-bit; Mobile and Mobile Enterprise are not supported)

Software

  • Adobe Reader®

More information

You will find more information at www.siemens.com/sinutrain.

Technical support

109756534

Preferably: https://support.industry.siemens.com/My/ww/en/requests#createRequest

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.