×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109757711, Entry date: 06/14/2018
(2)
Rate

SIMATIC PCS 7 Advanced Process Graphics V9.0 SP1

  • Entry
  • Associated product(s)
A service pack 1 is available for PCS 7 Advanced Process Graphics (APG) V9.0.

What's new?
PCS 7 Advanced Process Graphics V9.0 SP1 contains the following extensions or corrections:

  • "Quad View" enables the combination of up to 4 process pictures into an overview picture.

  • The "Group View" supports more types from the APL and IL.


A more detailed description of the extensions or corrections to previous versions can be found in the readme file.

Readme file
Refer the notes and compatibility statements in the readme file prior installation 109758333.

Installation instructions
The following installations are required for PCS 7 Advanced Process Graphics V9.0 SP1:
  • SIMATIC PCS 7 V9.0 SP1
  • PCS 7 Advanced Process Library V9.0 SP1
  • PCS 7 Advanced Process Graphics V9.0

Installation file
The following ZIP file contains the installation file.
 Registrierung notwendig SIMATIC PCS 7 Advanced Process Graphics V9.0 SP1 (29,4 MB) 

SHA-256 checksum: 5B6FE4E707676771BB209E8DF23496CEFC5D7081CEE39F411EF67AD0FCB6F257
Information on SHA-256

Order data

Designation

Order No.

PCS 7 Advanced Process Graphics V9.0
Engineering und Runtime license, valid for all ES, AS and OS of a SIMATIC PCS 7 project.

Form of delivery: Software and documentation on DVD, Certificate of License.

6DL5410-8BX58-0YA0

PCS 7 Advanced Process Graphics V9.0
Upgrade from V8.x to
 V9.0, valid for all ES, AS and OS of a SIMATIC PCS 7 project.

Form of delivery: Software and documentation on DVD, Certificate of License.

6DL5410-8BX58-0YE0

Note
In order to keep your system continuously up-to-date, please note the information in the compatibility tool: www.siemens.com/kompatool.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit