×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109757803, Entry date: 05/25/2018
(0)
Rate

SINAMICS V90: Generating a parameter backup using a SIMATIC function block

  • Entry
  • Associated product(s)
With the application example drive parameter sets of the V90PN can be saved to a SIMATIC S7-1200 and then subsequently send back to the drive.

This means that if a drive device has to be replaced, then the parameter set can be simply imported into the new device. This example shows how to store the drive dataset and how to import it into a new V90 device.

All necessary blocks will be described in the following document and are available in the project example. It is also possible to use it with a S7-1500 controller.







Downloads

  Manual Parameter Backup SINAMICS V90  (1,3 MB) 

Example projects
 Registrierung notwendig  Example project TIA V14SP1 (976,7 KB)
 Registrierung notwendig  Example project TIA V15 (1,0 MB) 


Additional Keywords

motioncontrol_apc_applications


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.