×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109757994, Entry date: 12/13/2018
(2)
Rate

Applicative conversion from 3SE6806 magnetic switch evaluation unit to 3SK2

  • Entry
  • Associated product(s)
This entry contains information about conversion of 3SE6806 to 3SK2

QUESTION:

What is the procedure when replacing the 3SE6806 safety relays?

 

 

ANSWER:

The 3SE6806 safety relays cannot be used with new applications. The software-parameterizable 3SK2 safety relays can be used for the same application.


The procedure for converting from 3SE6806 to 3SK2 is described in this document. In order to make the conversion process as fast and easy as possible, the following explanations are based on a template project in which the internal switching logic is already integrated.

  FAQ_109757994_Applicativeconversionfrom3SE6806to3SK2_V1_0_EN.pdf (1,3 MB) 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.