×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109758216, Entry date: 10/30/2018
(1)
Rate

Updates for SIRIUS SOFT STARTER ES V15

  • Entry
  • Associated product(s)
Available downloads: Overview of the current and earlier versions

Current version

Status October 2018: Update 2

This update is valid for the following product:

  • SIRIUS SOFT STARTER ES V15

In conjunction with PROFINET devices Note the following:

Devices connected to an enterprise network or directly to the internet must be appropriately protected against unauthorized access, e.g. by use of firewalls and network segmentation. For more information about industrial security, please visit http://www.siemens.com/industrialsecurity

Changes in SIRIUS Soft Starter ES V15 Update 2

  • Support of the new SIRIUS soft starter family 3RW5:
    • Soft Starter 3RW55 Basic Unit V1.0

    • HMI Module High Feature V1.1

    • PROFINET standard communication module V1.0 (Caution: To be able to use this communication module with 3RW55 the precondition is version 1.0.1)

    • PROFIBUS communication module V1.0 (Caution: To be able to use this communication module with 3RW55 the precondition is version 1.0.1)
    • MODBUS TCP communication module V1.0
  •  3RW44:
    • In the parameter editor you can induce to download the device name and/or the IP parameters. The IP parameters themselves can be set in the property tab in the inspector window.

    • To be able to use all features of SIRIUS Soft Starter ES V15, e.g. the expert list, you have to update the module description after upgrading a project to V15. This you can perform via the button “Update module description” in the inspector window.  Now this is possible for starters without a communication module

    • Improvements in the expert list and at the mass engineering

    • The trippings and events are sorted chronologically in the log book.

    • The colored bar charts of the current limits are displayed correctly after a language change.

  • General:
    • The trace configuration can be exported while the engineering trace is running.

    • Now it is also possible to use a calculated signal in trace without restrictions

Installation instructions:

  • Updates are cumulative and contain all previous updates.

  • The update can only be installed if SIRIUS SOFT STARTER ES V15 is already installed 109753470

  • After each installation of SIRIUS SOFT STARTER ES V15, the latest update needs to be installed.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the ReadMe_OSS file.

Special information for resellers

The information and the license terms in the ReadMe_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Readme_OSS.zip (3,8 MB)

Download

 Registrierung notwendig  SOFTSTARTER_ES_V15_Upd2.exe (252,6 MB)

SHA-256 checksum:  Registrierung notwendig  Code_SOFTSTARTER_ES_V15_Upd2.txt (1 KB)
Information about SHA-256: 109483101


Status June 2018: Update 1

This update is valid for the following product:

  • SIRIUS SOFT STARTER ES V15

In conjunction with PROFINET devices Note the following:

Devices connected to an enterprise network or directly to the internet must be appropriately protected against unauthorized access, e.g. by use of firewalls and network segmentation. For more information about industrial security, please visit  http://www.siemens.com/industrialsecurity 

Bug-fixing:

  • Improvements in the expert list
  • The reading of the trace data from the starter can take a few minutes. This process can be cancelled if it was started by mistake.
  • In the engineering trace the configuration can be exported even if the recording is running.
  • Openness: The attributes Typeidentifier and TypeName are returned back correctly.
  • The user can connect to a starter on which a configuration was downloaded which contains an older firmware than the starter has in fact.
  • The colored bars for the clear display of important parameters which were changed are shown correctly after opening a project.

Installation instructions:

  • Updates are cumulative and contain all previous updates.
  • The update can only be installed if SIRIUS SOFT STARTER ES V15 is already installed 109753470 
  • After each installation of SIRIUS SOFT STARTER ES V15, the latest update needs to be installed.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the ReadMe_OSS file.

Special information for resellers

The information and the license terms in the ReadMe_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Rate entry
no rating
Requests and feedback
What do you want to do?