×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109758423, Entry date: 09/22/2020
(2)
Rate

SINAMICS S120 firmware version 5.1 SP1 HF8

  • Entry
  • Associated product(s)
You can find a description of the SINAMICS S120 firmware version 5.1 SP1 HF8 here.

Description

The version designation on the memory card (CF) is SINAMICS S120 V05.01.01.08
The internal version number of the firmware is SINAMICS S120 V05.10.40.17

When upgrading, please observe the instructions for the firmware update.

Functional content and hardware support

A slide with the description of the most important functional contents can be found in Product notification 109758421.

Third-party software license conditions and copyright information

You can find the copyright information on the third-party software contained in this product, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the READ_OSS.HTM file.

Special note for resellers

The notes and the license conditions contained in the READ_OSS.HTM file must be passed on to the purchaser in order to avoid the reseller and purchaser from violating the licensing conditions.

Availability of the source code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information either directly on the product itself or with the product (e.g. on a mass storage medium, DVD). Should this not be possible due to technical reasons, Siemens will send you this OSS Source Code against payment of the handling expenses. Please contact the address specified at the end of this section regarding this matter.

Siemens AG 
Digital Factory
Customer Services DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555
90475 Nuernberg, Germany
Internet: http://www.siemens.com/automation/support-request
Tel.: +49 (911) 895-7222

 Registrierung notwendig  ReadMe_OSS.zip (399.0 KB) 

Supplementary conditions and functional restrictions

 Registrierung notwendig  SINAMICS_V5_1_SP1_Randbedingungen_en.pdf (6,1 KB)

Corrected functional restrictions

 Registrierung notwendig  S120_Corrected_Functional_Restrictions_V5_1_SP1_HF_en.xlsx (27,4 KB)

Instructions to update the firmware of the SINAMICS S120 CU320-2 and CU310-2

 Registrierung notwendig  Instructions_Firmware_Update_S120.doc (2,0 MB)

SINAMICS S120 firmware version 5.1 SP1 HF8 for the CU320-2 and CU310-2

 Registrierung notwendig  SINAMICS_S120_FW_V5_1_1_HF8.zip (119,4 MB)

As of version 4.7 HF7, the SINAMICS S120 Runtime firmware as download is not subject to any export restrictions, as the output frequency has been limited to 550 Hz.

It is not subject to the Iran embargo, and is not listed in the EC Dual Use regulation. (AL = N).
It is not a US product (ECCN = N).

If higher output frequencies are required, then the "High output frequency" license must be purchased, article no.: 6SL3074-0AA02-0AA0. It can also be ordered as Z option J01 together with the CF card, see 104020669.

The "High output frequency" license is subject to export restrictions, and currently has export code: AL:3E225, ECCN: N SH code: 0.

Alternatively, a new memory card (CF) with the following article number can be used:

  • Without performance expansion: Article no.: 6SL3054-0FB10-1BA0
  • With performance expansion firmware option: Article no.: 6SL3054-0FB11-1BA0

List of faults and alarms

The "alarmlist_*.xml" are not necessary for the correct operation of the firmware and the associated STARTER. They only contain a text-based export of the "Alarm messages" of the S120 in the "xml" format (this format guarantees a correct text-based representation, independent of the wide range of fonts that exist worldwide; this means that they can be converted error-free into other formats).
 This text-based export is occasionally requested by customers to process them further in their own applications respectively load them onto external devices. As a consequence, as far as the S120 product is concerned, no additional support can be provided here.

 Registrierung notwendig  S120_V5_1_SP1_alarmlist.zip (2.5 MB) 

GSD files for project integration in PROFIBUS configuration tools

The PROFIBUS GSD files are saved on the SINAMICS S120 CompactFlash card under the following path: ..\SIEMENS\SINAMICS\DATA\CFG
However, they can also be downloaded at 49216293 .

GSDML files for project integration in PROFINET configuration tools

The PROFINET GSD files are saved on the SINAMICS S120 CompactFlash card under the following path: ..\SIEMENS\SINAMICS\DATA\CFG
However, they can also be downloaded at 49217480 .

EDS files for project integration in CANopen configuration tools

see 48802094.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.