×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109758500, Entry date: 10/29/2018
(1)
Rate

Updates for SIMOCODE ES V15 (TIA Portal)

  • Entry
  • Associated product(s)
Available downloads: Overview of the current and earlier versions.

Current version


Status November 2018: Update 2 

This Update is valid for the following products:

SIMOCODE ES V15 Basic
SIMOCODE ES V15 Standard
SIMOCODE ES V15 Premium

Improvements and fixed issues in SIMOCODE ES V15 Update 2

  • Support of new SIMOCODE pro base units
    • SIMOCODE pro V GP1 V2.1
    • SIMOCODE pro V GP2 V2.1
    • SIMOCODE pro V PN V2.1
  • Support of new Current/voltage measuring modules for dry-running protection. Set-up of dry-running protection parameters with help of the dry-running protection wizard.
  • Fixed issues after upgrading V13 projects.
  • SIMOCODE pro V EIP devices can now configure outputs for acyclic send date.
  • Cyclic send data from bytes 4-9 are not displayed after migration of SIMOCODE ES 2007 project files.

Installation instructions:
  • Please make sure that further TIA Portal V15 based software products have at least the Version V15 Update 2. Otherwise, installation of SIMOCODE ES V15 Update 2 is not possible.
  • The update can only be installed if SIMOCODE ES V15 (TIA Portal) is already installed.
  • After each installation of SIMOCODE ES V15 (TIA Portal) , the latest update needs to be installed.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS file.

Special information for resellers

The information and the license terms in the  Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Readme_OSS.zip (1,1 MB)

Download

 Registrierung notwendig  SIMOCODE_ES_V15_Upd2.exe (225,1 MB)
SHA-256 checksum:   Registrierung notwendig  Code_SIMOCODE_ES_V15_Upd2.txt (1 KB)
Information about SHA-256: 109483101


Status June 2018: Update 1

This Update is valid for the following products:

SIMOCODE ES V15 Basic
SIMOCODE ES V15 Standard
SIMOCODE ES V15 Premium

Improvements and fixed issues in SIMOCODE ES V15 Update 1

  • Fixed issues for migrating from SIMCOCODE ES 2007: The parameter settings for analog values of Cyclic send data are now migrated properly.
  • When “cold run” feature was active, it was not possible to force the input signals of the logic module “Analog multiplexer”
  • Corrected parameters settings for the response on open circuit within input range of 0 to 20mA of the analog module.
  • With SIMOCODE pro V ModBus base units the parameters for Operator panel with display were not visible.
  • The parameter wizard did not show all settings when no license was given.
  • Corrected parameters settings for warning and trip level of the monitoring function “internal ground fault” of the current/voltage measuring module V2.
  • If the error buffer was not fully filled with log entries the text “Hardware fault basic unit” was shown instead of empty lines. Furthermore a “temporary fault” was shown instead of “Hardware fault basic unit”.
  • After parameter upload from SIMOCODE pro V PN V2.0 with current/voltage measuring module V1.0 with activated internal earth fault detection the compiler complained about wrong settings for warning and trip level.
  • Forced measured values of type “Float” are now shown correctly in test dialog.
  • Corrected compile error after upgrading Step7+ V13 projects with DM-F PROFIsafe digital modules.

Installation instructions:

  • Please make sure that further TIA Portal V15 based software products have at least the Version V15 SP1 Update 2. Otherwise, installation of SIMOCODE ES V15 Update 1 is not possible. 

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS file.

Special information for resellers

The information and the license terms in the  Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Readme_OSS.zip (1,2 MB)

Download

 Registrierung notwendig  SIMOCODE_ES_V15_Upd1.exe (191,7 MB)
SHA-256 checksum:   Registrierung notwendig  Code_SIMOCODE_ES_V15_Upd1.txt (1 KB)
Information about SHA-256: 109483101

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.