×
Siemens Industry Online Support
Siemens AG
Type de contribution : Télécharger ID de la contribution : 109758848, Date de la contribution : 26/10/2018
(2)
Évaluer

TRIAL Download SIMATIC S7-PLCSIM Advanced V2.0 SP1

  • Contribution
  • Concerne le/les produits(s)
The Trial download of the V2.0 SP1 of SIMATIC S7-PLCSIM Advanced is available effective immediately (October 26, 2018).

SIMATIC S7-PLCSIM Advanced enables you to create virtual controllers for simulating S7-1500 and ET 200SP controllers and provides extensive simulation of functions.


Highlights SIMATIC S7-PLCSIM Advanced V2.0 SP1: 
  • Support of the firmware 2.6
  • Possibility to adapt the max. cycle time through  the API
  • Support of the PN/PN coupler (F-Send / F-Receive)
  • Control Panel als free floating window, which allows you to:
    • Move the floating window around freely
    • Drag and drop instances from an explorer window to the control panel
    • Pin the Control Panel to the desktop (always on top)

Readme file:

You can find additional information on SIMATIC S7-PLCSIM Advanced V2.0 SP1 in the attached Readme file. You can view this file in the portable document format (.pdf):

  s7plcsim_advanced_readme_en-US.pdf (566,5 KB)

System requirements:

SIMATIC S7-PLCSIM Advanced V2.0 is released for use with the following operating systems:

  • Windows 7 Home Premium SP1
  • Windows 7 Professional SP1
  • Windows 7 Enterprise SP1
  • Windows 7 Ultimate SP1
  • Windows 10 Home Version 1709 and 1803
  • Windows 10 Pro Version 1709 and 1803
  • Windows 10 Enterprise Version 1709 and 1803
  • Windows 10 (IoT) Enterprise 2016 LTSB
  • Windows Server 2012 R2 Standard (complete installation)
  • Windows Server 2016 R2 Standard (complete installation)

The following table shows the recommended hardware for the operation of SIMATIC S7-PLCSIM Advanced V2.0:

HardwareVirtual Machine
 Processor
  • One logical Intel Core i7-6820EQ core per started instance
  • At least one additional core for the operating system
  • At least one additional core for the accitional active applicationjs
  • One virtual CPU per started instance to be assigned to the virtual machine
  •  A corresponding number of processors has to be physically available on the host
  • At least one additional core for the operating system
  • At least one additional core for the additional active applications
 RAM
  • 1GB per started instance
  • At leat 4GB for the Windows operating system
  • Additional RAM corresponding to the requirements of the remaining active applications
  • 1GB per started instance
  • At leat 4GB for the Windows operating system
  • Additional RAM corresponding to the requirements of the remaining active applications
 Hard disk min. 5GB free hard disk space min. 5GB free hard disk space

 Screenresolution

 min. 1024 x 768 min. 1024 x 768
 

Supported virtualization platforms:

  • VMware vSphere Hypervisor (ESXi) 6.5
  • VMware Workstation Professional 12.5.5
  • VMware Workstation Player 12.5.5

Notes about downloading:

The software is subject to export restrictions. Therefore, download is only possible for registered users. Please note that, on account of the strong demand, the registration for export-restricted downloads will take some time.

As a registered customer, you can download the trial version of SIMATIC S7-PLCSIM Advanced V2.0 and test it for 21 days.

Additional information on the trial software for the products in TIA Portal V15 is also available in the following entry: 109761045


SIMATIC S7-PLCSIM Advanced V2.0:

 Registrierung notwendig  SIMATIC_PLCSIM_Advanced_V2_SP1.exe (639,8 MB)

SHA-256 checksum:

 Registrierung notwendig  SIMATIC_PLCSIM_Advanced_V2_SP1.txt (1 KB)

Information on SHA-256 can be found here 109483101.



Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity. 




Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport