×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109759381, Entry date: 08/17/2018
(1)
Rate

Delivery release for SINAMICS Startdrive V15 Update 3

  • Entry
  • Associated product(s)
Update 3 for SINAMICS Startdrive V15 has been released for delivery.

Update 3 for SINAMICS Startdrive V15 is available under 109754382 and includes improvements, particularly in the following areas:

  • Control panels
  • Working in the list of accessible nodes
  • Telegram configuration
  • EPos
  • Online parameterization

SINAMICS Startdrive V15 Update 3 applies to Startdrive Basic and Startdrive Advanced.

Previous updates

Update 3

  • can only be installed if Startdrive V15 is already installed.
  • includes Update 2. Update 1 is not included and must be installed separately.

Installation instructions

Update 3 must be installed after the installation of SINAMICS Startdrive V15.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.