×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109759477, Entry date: 07/27/2018
(0)
Rate

Software SIMOCODE pro PCS 7 Library V8.3

  • Entry
  • Associated product(s)
The software SIMOCODE pro PCS 7 Library V8.3 is now available for download. With this download, an existing installation of SIMOCODE pro PCS 7 Library V8.1 or V8.2 can be updated to V8.3. The use of the software SIMOCODE pro PCS 7 Library V8.3 requires as a minimum SIMATIC PCS 7 V8.1.

What is new in V8.3?

New Features

  1. Support for SIMOCODE proV V4.0 and SIMOCODE proV PN V2.0 along with its new features.
  2. Support for UM+ (2nd Generation current/voltage) range of modules.
  3. Detection of UM+ module, Digital Module1 and 2 – Bi stable, Digital Module1 and 2 – Mono, Earth-fault module 2 (EM+).
  4. New device diagnostic events at Operation faceplate.
    • Internal Earth Fault
    • BU FW Update Active
    • Module FW Update Active.
  5. New error type message related to FW Update and HW Fault is now available at Logbook faceplate with timestamp 
  6. Frequency and Average Current Detection in Measurement faceplate.
  7. Consumed Energy at Statistical faceplate is displayed now as float values with 2 decimals.
  8. Higher precision Float values display with 2 decimal for the following parameters at Measurement faceplate along with Cyclic reading.
    • Frequency
    • Current I_max
    • Current I_Avg
    • Current I_L1
    • Current I_L2
    • Current I_L3
    • Active Power
    • Apparent Power
    • Voltage UL1
    • Voltage UL2
    • Voltage UL3
    • Cos-Phi

Bug Fixes

  1. Code has been optimized to prevent WinCC runtime from crash during reading Logbook events using "Read data" button

  2. Problem with Trend view in Web Client has been fixed.

  3. During group error/warning there will be message text shown for coming events but not for going events, this issue has been solved.

  4. Module Fault and Rack Fault diagnostics has been fixed in line with OB_DIAG1_PN S2 redundancy handling.

  5. Incorrect MODE value reporting during device disconnection at MMDiag, MMOprtn blocks is fixed.

  6. OB_DIAG1.QRACK false error report on device unavailability behind Y-link and Rack fault outgoing event was corrected.

  7. Device failure is reported when PORT diagnostic is activated and one end of the ring network is removed from a MRP configuration with SCALANCE.

  8. OB_DIAG1 not reporting QRACKF high, when Y-Link (connected to CPU) is turned OFF.

  9. Read data button is enabled even if the OS permission disabled when the faceplate is open, this issue has been fixed at MMOprtn and MMLog faceplates.

  10. SUBN1ERR & SUBN2ERR toggles in OB_DIAG1 for the slaves connected to communication processor (CP443-5) in standard master system

  11. Unit of Consumed energy parameter at MMStat Standard faceplate is not grayed out when Voltage module is not available; this issue is fixed at MMStat faceplates.

  12. In MMMeas faceplates Analog module 2 sensor 2 will be visible even though the Analog module 2 is not configured

  13. OB_DIAG1.QRACKF shows false error behind communication processor CP443-5 in standard master system

  14. OB_DIAG & MMDiag block not behaving as expected on Y-Link with communication processor CP443-5 card, this behavior is now corrected.

  15. Date column should not come in case of Profibus in Logbook faceplates.


Installation notes:

Please observe the description of new features and alterations, the installation and application notes available in the file MMReadme.zip which can be downloaded here:

 Registrierung notwendig  MMReadme.zip (50,4 KB)

SIMOCODE pro PCS 7 Library V8.3 is offered in the form of the download file „SIMOCODE_pro_PCS7_Library_V82_V83.exe“. Please first download this file and then execute it. Afterwards, the file will be extracted and you can execute the setup. Please exit all STEP 7 applications prior to starting the installation.


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS.zip file.

Special information for resellers

The information and the license terms in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  readme_oss.zip (12,2 KB)


Download

 Registrierung notwendig  SIMOCODE_pro_PCS7_Library_V82_V83.exe (709,2 MB)

SHA-256 checksum:    Registrierung notwendig  Code_SIMOCODE_pro_PCS7_Library_V82_V83.txt (1 KB)
Information about SHA-256:  109483101

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.