×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109759617, Entry date: 10/26/2018
(4)
Rate

Delivery release STEP 7 Safety Basic / Advanced V15.1

  • Entry
  • Associated product(s)
Delivery release for SIMATIC STEP 7 Safety Basic / Advanced V15.1, the high-performance add-on package for programming of fail-safe S7 controllers for the Totally Integrated Automation Portal V15.1.

SIMATIC STEP 7 Safety V15.1 is now available. SIMATIC STEP 7 Safety V15.1 replaces the direct predecessor version SIMATIC STEP 7 Safety V15 as an independent product and full version. The standard delivery of SIMATIC STEP 7 Safety V15 ends with the availability of SIMATIC STEP 7 Safety V15.1.

SIMATIC STEP 7 Safety V15 can be requested as a free download to the previously delivered version V15.1 via the Internet from the download pages of SIMATIC Customer Support (entry ID 109752230).

The license acquired for the V15.1 is valid for all older TIA Portal versions.


If you need the V15.0 volume, the TRIAL Version of V15.1 (MLFB: 6ES7833-1FA15-0YA8) contains the V15.0 DVD.


The TIA Portal add-on package SIMATIC STEP 7 Safety Basic / Advanced convinces with numerous new engineering features and supports the extended portfolio of S7-1500F and S7-1200F.

  • STEP 7 Safety Basic V15.1 is the add-on package for parameter assignment and programming of the fail-safe S7-1200.
  • STEP 7 Safety Advanced V15.1 is the add-on package for all fail-safe TIA SIMATIC controller classes (S7-1500, S7-1200, S7-1500 Software Controller, S7-300, S7-400, WinAC).


You can find additional information for the TIA Portal software in the following entry:
TIA Portal V15.1 (109758794)


Highlights


  • New fail-safe CPU-CPU communication "Flexible F-Link"

With STEP 7 Safety V15.1, a new fail-safe CPU-CPU communication "Flexible F-Link" is available for the fail-safe S7-1200 and S7-1500 CPUs. This enables fail-safe data to be easily exchanged between two fail-safe CPUs as a fail-safe array using standard communication mechanisms.

Flexible F-Link offers several advantages for exchanging fail-safe data:

  • Grouping of the fail-safe data to be transferred into F-conformant PLC data types (UDTs)
  • Up to 100 bytes of fail-safe data per UDT
  • Support of fail-safe data types
  • Easy parameter assignment and automatic generation of fail-safe communication DBs
  • Transfer of fail-safe data with standard communication blocks even across network boundaries
  • F-runtime group communication for F-CPUs 1200/1500
  • System-integrated and worldwide sufficiently unique F-Communication UUID
  • Separate F-communication address signature for easy recognition of changes of the F-communication UUID



  • F-OB preprocessing and postprocessing
To simplify configuring and for easy-to-follow timing, especially in the context of fail-safe communication using Flexible F-Link, STEP 7 Safety Version V15.1 provides the option of placing standard blocks around the F-runtime groups for the purpose of preprocessing and postprocessing process values.


  • Variable communication ID (DP_DP_ID)
Starting in Version V15.1, STEP 7 Safety provides the option of assigning variables instead of constants to the communication IDs (DP_DP_IDs) needed for the SENDDP and RCVDP blocks. This allows use of safety programs with the same collective F-signature in systems with a variety of identical I-devices.  The variable communication ID thus enables simplified commissioning, maintenance and project management.

Notice: If variable communication IDs (DP_DP_ID) are used, the user must ensure by the application that the communication IDs are always unique throughout the network.


  • New openness functionalities
  • Reading/configuring of I-parameters of the ET 200SP F-IOs
  • Consistent station upload
  • HW/SW comparison (offline/offline)
  • Import/export of consistent F-blocks and F-conformant PLC data types (UDT)


  • Simulation mode for SENDDP / RCVDP during S7-PLCSIM operation


  • Achievable safety class SIL3 (Safety Integrity Level) according to IEC 61508:2010 / PL e (Performance Level) according to ISO 13849-1:2015



Investment protection

Starting from STEP 7 Safety V13 SP1, projects can be upgraded directly to STEP 7 Safety V15.1.

Projects from older versions of STEP 7 Safety (V11 to V13) are updated based on STEP 7 Safety Advanced V13 SP1 or V13 SP2 (most recent update recommended).

You can download Service Pack 2 for SIMATIC STEP 7 Safety Basic / Advanced V13 under the following entry ID:


Important note:
TIA Portal project versions V13 SP1 to V15 are upgraded with TIA Portal V15.1 to project version V15.1. If you need to edit a TIA Portal project version V13 SP1 to V15, we recommend an additional installation of the corresponding software for TIA Portal V15.1. The license purchased for V15.1 is also valid for all older TIA Portal versions.


S7 Distributed Safety V5.4 SP5 projects can be migrated to STEP 7 Safety Advanced V15.1 by migrating the program code and hardware configuration.



System requirements and compatibility with other SIMATIC products

  • STEP 7 Safety Advanced V15.1 requires STEP 7 Professional V15.1 (109758795)
  • STEP 7 Safety Basic V15.1 requires at least STEP 7 Basic V15.1 (109758795)


Refer to STEP 7 Professional V15.1 for the supported operating systems and hardware requirements. The compatibility with other SIMATIC products is the same as for STEP 7 Basic / Professional V15.1.



Software Update Service (SUS)

SUS S7 Distributed Safety and Safety Basic/Advanced:

  • Customers that have an existing Software Update Service agreement for S7 Distributed Safety or Safety Advanced receive an upgrade to STEP 7 Safety Advanced V15.1 within the framework of their agreement upon delivery release of STEP 7 Safety Advanced V15.1.
  • Customers that have an existing Software Update Service agreement for Safety Basic receive an upgrade to STEP 7 Safety Basic V15.1 within the framework of their agreement upon delivery release of STEP 7 Safety Basic V15.1.

Delivery takes place automatically.

You can find additional information about the Software Update Service here.



Trial software download

Here you can download a trial version of SIMATIC STEP 7 Safety Advanced V15.1 and test it for 21 days: 109759618 



Readme file

You will find additional information on STEP 7 Safety Basic/Advanced V15.1 in the accompanying Readme file. You can view this file in the portable document format (.pdf).

 Registrierung notwendig  ReadmeFAIL_de_en_V15_1.pdf (237.2 KB)


Informational material

  • Online Support - Technical information on the TIA Portal, entry ID: 65601780
  • Programming Guideline for S7-1200 / S7-1500: Entry ID: 67582299
  • Comparison list for programming languages: Entry ID:  86630375



Ordering data

Designation

Article no.

STEP 7 Safety Advanced V15.1

6ES7833-1FA15-0YA5

STEP 7 Safety Advanced V15.1
Software download 

6ES7833-1FA15-0YH5

Upgrade**
STEP 7 Safety Advanced V11 to V14 (Combo) -> V15.1 (Combo) or

Distributed Safety V5.4 -> V15.1 Combo

6ES7833-1FA15-0YF5

Upgrade**
STEP 7 Safety Advanced V11 to V14 (Combo) -> V15.1 (Combo) or

Distributed Safety V5.4 -> V15.1 Combo

Software download

6ES7833-1FA15-0YY5

Trial***
STEP 7 Safety Advanced V15.1

6ES7833-1FA15-0YA8

SUS STEP 7 Safety Advanced - Standard*

6ES7833-1FC00-0YX2

SUS STEP 7 Safety Advanced - Compact *

6ES7833-1FC00-0YM2

SUS STEP 7 Safety Advanced - Download*

6ES7833-1FC00-0YY0

STEP 7 Safety Basic V15.1

6ES7833-1FB15-0YA5

STEP 7 Safety Basic V15.1
Software download

6ES7833-1FB15-0YH5

Upgrade
STEP 7 Safety Basic V13 SP1 to V14 -> V15.1

6ES7833-1FB15-0YE5

Upgrade 
STEP 7 Safety Basic V13 SP1 to V14 -> V15.1
Software download

6ES7833-1FB15-0YK5

Powerpack
STEP 7 Safety Basic V15.1 -> STEP 7 Safety Advanced V15.1

6ES7833-1FA15-0YC5

Powerpack
STEP 7 Safety Basic V15.1 -> STEP 7 Safety Advanced V15.1
Software download

6ES7833-1FA15-0YJ5

 SUS STEP 7 Safety Basic - Standard*

6ES7833-1FD00-0YX2

 SUS STEP 7 Safety Basic - Compact*

6ES7833-1FD00-0YM2

 SUS STEP 7 Safety Basic - Download*

6ES7833-1FD00-0YN2

Delivered from stock Nuremberg Logistics Center LZN


* You can find additional information about the Software Update Service here.

** This product also includes software version V13 SP2. The license key for V15.1 can also be used for V15, V14, V13, V12 and V11.

*** Delivery also includes STEP 7 Safety Advanced V15 DVD


Download ordering data:

 Registrierung notwendig  Step_7_Safety_v15_1_order_list.xls (33.5 KB)








Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit