×
Siemens Industry Online Support
Siemens AG
文档类型 常问问题 文档编号 109760164, 文档发布日期 2018年8月23日
(0)
评估

Use of PROFINET standard or PROFIBUS communication module with the SIRIUS 3RW55 soft starter

  • 文档
  • 涉及产品
This entry contains information about the use of a PROFINET standard or PROFIBUS communication module with the SIRIUS 3RW55 soft starter.

QUESTION:

Which steps are necessary to use a communication module (PROFINET standard or PROFIBIUS) with the SIRIUS 3RW55 soft starter?

 

 

ANSWER:

For operation of a SIRIUS 3RW55 soft starter together with a communication module PROFINET standard (article number: 3RW5980-0CS00) or PROFIBUS (article number: 3RW5980-0CP00) a firmware update of the communication module to version V1.0.1 or higher is necessary.
Download via 3RW5 topic page 
in Siemens Industry Online Support (SIOS).
(as soon as GSD, GSDML and SIRIUS Soft Starter ES for 3RW55 is available)
安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。