×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109760217, Entry date: 02/22/2019
(0)
Rate

Function blocks and faceplates for evaluation of the diagnostic interface "COM" and visualization of the device data

  • Entry
  • Associated product(s)
The SITOP PSU6200 power supply has a diagnostic interface "COM" whose signal can be evaluated via a digital input in a higher-level controller, e.g. S7-1200 CPU and S7-1500 CPU.

The diagnostic interface "COM" of the PSU6200 provides a signal that transmits the following device data as a Manchester code:

  • Voltage and current values
  • Nominal data
  • Device information
  • Temperature and operating hours

Solution
The following library provides function blocks for SIMATIC S7-1200/S7-1500 and faceplates for SIMATIC Comfort Panels. The function blocks enable you to read in and evaluate the signal of the diagnostic interface "COM" via a digital input at the S7-CPU. You can use the faceplates to clearly display the device data on an HMI control panel.

Note
The library blocks for SIMATIC S7-1500 can also be used in an ET 200SP CPU and ET 200pro CPU.

The following image shows the graphic representation of the solution.


Fig. 1

No.Description
1Power supply
2CPU with function block (FB)
3Digital input module (DI) 
4diagnostic interface "COM" 
5Output 24 V DC 
6Input 230 V AC 

Table 1

Library
  Documentation Library "LPSU6200_V15.0-0_V1-0-0" (3,0 MB)
 Registrierung notwendig  Library for STEP 7 V15 (2,7 MB)

Last Changes  
Add function block and faceplates for S7-300 / S7-400


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.