×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109760217, Entry date: 08/16/2019
(4)
Rate

Function blocks and faceplates for evaluation of the diagnostic interface "COM" and visualization of the device data

  • Entry
  • Associated product(s)
The SITOP PSU6200 power supply has a diagnostic interface "COM" whose signal can be evaluated via a digital input in a higher-level controller, e.g. S7-1200 CPU, S7-1500 CPU and S7-300 CPU / S7-400 CPU.

The diagnostic interface "COM" of the PSU6200 provides a signal that transmits the following device data as a Manchester code:

  • Voltage and current values
  • Nominal data
  • Device information
  • Temperature and operating hours

Solution
The following library provides function blocks for SIMATIC S7-1200, S7-1500, S7-300, S7-400 and faceplates for SIMATIC Comfort Panels. The function blocks enable you to read in and evaluate the signal of the diagnostic interface "COM" via a digital input at the S7-CPU. You can use the faceplates to clearly display the device data on an HMI control panel.

Note

  • The library blocks for SIMATIC S7-1500 can also be used in an ET 200SP CPU and ET 200pro CPU.
  • The library blocks for SIMATIC S7-300 can also used in an ET 200S CPU and ET 200pro CPU.

The following image shows the graphic representation of the solution.


Fig. 1

No.Description
1Power supply
2CPU with function block (FB)
3Digital input module (DI) 
4diagnostic interface "COM" 
5Output 24 V DC 
6Input 230 V AC 

Table 1

Library
  Documentation Library "LPSU6200_V15.0-0_V1-1-0" (3,2 MB)
 Registrierung notwendig  Library for STEP 7 V15 (1,6 MB)

Last Changes  
Set and display status and default values in case of communication with diagnostic interface "COM" is not active.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.