×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109760324, Entry date: 08/30/2018
(5)
Rate

Release / Download TeleControl Server Basic V3.1 + Update 1 (V3.1.0.1) for Demo Mode

  • Entry
  • Associated product(s)
This provides the TeleControl Server Basic (TCSB) V3.1.0.1 control station software for operation in demo mode for download. An appropriate license of the current software must be purchased for full use.

The TeleControl Server Basic software connects up to 5,000 SIMATIC remote terminal units (RTUs) to a control center via mobile wireless and Ethernet / Internet. Connection to the client takes place via OPC UA or OPC DA. This allows telecontrol solutions to be economically implemented in the fields of water/wastewater, logistics, maintenance and energy optimization.

 

The following operating systems have been released for TCSB V3.1 + Update 1:

  • Windows 10 Pro, Enterprise V1703, V1709, V1803 (64-bit)

  • Windows 8.1 Pro (64-bit)

  • Windows 7 Pro, Ultimate, Enterprise + SP1 (64-bit)

  • Windows Server 2016 Standard, Datacenter V1607 (64-bit)

  • Windows Server 2012 R2 Standard (64-bit)

  • Windows Server 2008 R2 Standard + SP1 (64-bit)  

TCSB V3.1 has been tested with WinCC V7.3 and V7.4.

 

Notes for TCSB operation in demo mode:

If no license to use this program is purchased, the program runs in demo mode. This enables operation of a connection from the TCSB to a telecontrol station / RTU. If you activate multiple connections, you will see notes on licensing.

Copying and/or distributing the program is not permitted. Furthermore, the user is not permitted to decompile and/or edit, change or integrate the program into other programs. The use of the program in demo mode is at your own risk and is not suitable for productive operation.

Please note: There is no technical support via the Siemens hotline for programs that are operated in demo mode. A valid license is required for this.

 

TCSB license:

Information about the control station software TeleControl Server Basic V3.1.0.1 can be found here: 109757071 

 




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.