Entry type:
Download
Entry ID:
109760397,
Entry date:
09/03/2018
Rate
Patch 01 for Evaluation Kit EK-ERTEC 200 PN IO Firmware V4.5
-
Entry
-
Associated product(s)
Patch 01 for PROFINET IO evaluation kit version 4.5.0, concerning EK ERTEC200 is released
The following fixes affect the PNIO stack:
- Problem at submodule-plugging in special case of IM data configuration.
- Wrong response “invalid index” instead of “access denied” if submodule has no own IM data.
- HW revision in IM0 data contains ERTEC version value instead of value provided from application at submodule plugging.
- Sporadically IO data update provides data from last cycle to application
How to update the software for the EK ERTEC 200:
- Extract the zip file “EK_ERTEC200_V4.5.0_PATCH_01.zip”
- To be sure, make a backup of your source first !!
- Update all source files, header files and configuration files inside this fix on your installed version PNIODevkit\Pnio_src. You can do it with a simple copy, if you use the unchanged path structure of PNIO_src of the preliminary devkit version V4.5.0
Download
A password is required to unzip the file. Registered customers will receive the password from the ComDeC. comdec@siemens.com
EK_ERTEC200_V4.5.0_PATCH01.zip (22,8 KB)
Name: EK_ERTEC200_V4.5.0_PATCH01.zip
Size: 23338 bytes (22 KiB)
SHA256: 464FA46662B175300732626889923738CC2E683EE9CDABA5BF7C6F70638391B3
---------------------------
Checksum information: (How do you determine the SHA-256 checksum of a file?: 109483101
---------------------------
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Also available in the following languages:
- German
- Spanish
- Chinese
Entry belongs to product tree folder(s):
Rate entry
Feedback *)
Name
Phone number
email
DetailPages.Subject
Comment
Number of characters: 0 (max. 500)
Send copy of comment to sender. (login required)
*) Important: Please use this form for general feedback only. All technical and specialist topics should be directed to the expert community in the Technical Forum.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).
Copy URL
mySupport Cockpit
Product information
Topic pages for this entry