×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109760401, Entry date: 09/03/2018
(1)
Rate

Patch 01 for Evaluation Kit EK-ERTEC 200P PN IO Firmware V4.5

  • Entry
  • Associated product(s)
Patch 01 for PROFINET IO evaluation kit version 4.5.0, concerning EK-ERTEC 200P is released; valid for ASICs ERTEC 200P and ERTEC 200P-2

The following fixes affect the PNIO stack:

  • Problem at submodule-plugging in special case of IM data configuration.
  • Wrong response “invalid index” instead of “access denied” if submodule has no own IM data.
  • HW revision in IM0 data contains ERTEC version value instead of value provided from application at submodule plugging.

How to update the software for the EK ERTEC 200P:

  1. Extract the zip file “EK_ERTEC200P_V4.5.0_PATCH_01.zip”
  2. To be sure, make a backup of your source first!
  3. Update all source files, header files and configuration files inside this fix on your installed version PNIODevkit\Pnio_src. You can do it with a simple copy, if you use the unchanged path structure of PNIO_src of the preliminary devkit version V4.5.0

Download

A password is required to unzip the file. Registered customers will receive the password from the ComDeC. comdec@siemens.com

 Download unterliegt Exportcontrolle  EK_ERTEC200P_V4.5.0_PATCH01.zip (17,3 KB)

Name: EK_ERTEC200P_V4.5.0_PATCH01.zip
Size: 17666 bytes (17 KiB)
SHA256: EDF5A17AA615CDBEC9EC3CE93CAB45329515C65DB16883833DC9BAEB0B4E37FC

---------------------------

Checksum information: (How do you determine the SHA-256 checksum of a file?:109483101 

---------------------------

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.