×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109760470, Entry date: 09/14/2018
(1)
Rate

Download firmware SCALANCE W700 IEEE 802.11n V6.3.1

  • Entry
  • Associated product(s)
This firmware update V6.3.1 can be used for SCALANCE W700 IEEE 802.11n products and replaces the older firmware version V6.3.0 Affected article numbers (MLFB):

 

Product name

Article numbers (RoW)

Article numbers (US)

Article numbers (IL)

SCALANCE W721-1 RJ45

6GK5721-1FC00-0AA0

6GK5721-1FC00-0AB0

 

SCALANCE W722-1 RJ45

6GK5722-1FC00-0AA0

6GK5722-1FC00-0AB0

6GK5722-1FC00-0AC0

SCALANCE W734-1 RJ45

6GK5734-1FX00-0AA0

6GK5734-1FX00-0AB0

 

SCALANCE W738-1 M12

6GK5738-1GY00-0AA0

6GK5738-1GY00-0AB0

 

SCALANCE W748-1 RJ45

6GK5748-1FC00-0AA0

6GK5748-1FC00-0AB0

 

SCALANCE W748-1 M12

6GK5748-1GD00-0AA0

6GK5748-1GD00-0AB0

 

SCALANCE W761-1 RJ45

6GK5761-1FC00-0AA0

6GK5761-1FC00-0AB0

 

SCALANCE W774-1 RJ45

6GK5774-1FX00-0AA0

6GK5774-1FX00-0AB0

6GK5774-1FX00-0AC0

SCALANCE W774-1 M12 EEC

6GK5774-1FY00-0TA0

6GK5774-1FY00-0TB0

 

SCALANCE W778-1 M12

6GK5778-1GY00-0AA0

6GK5778-1GY00-0AB0

 

SCALANCE W778-1 M12 EEC

6GK5778-1GY00-0TA0

6GK5778-1GY00-0TA0

 

SCALANCE W786-1 RJ45

6GK5786-1FC00-0AA0

6GK5786-1FC00-0AB0

 

SCALANCE W786-2 RJ45

6GK5786-2FC00-0AA0

6GK5786-2FC00-0AB0

6GK5786-2FC00-0AC0

SCALANCE W786-2IA RJ45

6GK5786-2HC00-0AA0

6GK5786-2HC00-0AB0

 

SCALANCE W786-2 SFP

6GK5786-2FE00-0AA0

6GK5786-2FE00-0AB0

 

SCALANCE W788-1 RJ45

6GK5788-1FC00-0AA0

6GK5788-1FC00-0AB0

 

SCALANCE W788-2 RJ45

6GK5788-2FC00-0AA0

6GK5788-2FC00-0AB0

6GK5788-2FC00-0AC0

SCALANCE W788-1 M12

6GK5788-1GD00-0AA0

6GK5788-1GD00-0AB0

 

SCALANCE W788-2 M12

6GK5788-2GD00-0AA0

6GK5788-2GD00-0AB0

 

SCALANCE W788-2 M12 EEC

6GK5788-2GD00-0TA0

6GK5788-2GD00-0TB0

6GK5788-2GD00-0TC0

Reason for change:

  • Fix malfunction of LLDP frames at port 1 in SCALANCE W77x/W73x devices
  • Fix communication problems when using WEP and 'Auto Channel'
  • Fix sporadic device restart with access via SNMP to Load&Save configurations

Notes:

  • This version contains security-related improvements which increase ruggedness. We recommend performing an update.
  • iPRP: Undesired side effects can occur when using iPRP in combination with A-MPDU. We therefore recommend avoiding the simultaneous use of the two functions.
  • Incompatibility C-PLUG created with firmware V1.0: If a device including the C-PLUG is equipped with the firmware V1.0 and a defect occurs, the device can only be replaced by a device with firmware V6.0 or older. After the replacement the device can be updated to the current firmware version.
  • Incompatibility with iPRP: iPRP systems with version V6.0.0 are not compatible with devices with version V6.1.0. All devices must be brought to the same firmware version (V6.0.0 or higher V6.1.0).
  • Due to increasing security requirements, only the AES encryption method is supported with iPCF and iPCF-MC. As of V05.00.00, the WEP encryption method can no longer be configured. Note: Existing installations that use the non-secure WEP encryption method should be upgraded to the more secure AES encryption method. In any event, this upgrade must be carried out before a firmware update to V05.00.00.
  • Note: If an EDS file from V5.2.1 is used and the device with firmware V6.1.1 is running, the devices are no longer accessible online.
  • The transfer protocol IEEE 802.11b is not supported in combination with iPCF, which means the SCALANCE W700-xRR devices must not be configured with the IEEE 802.11b operating mode in mixed operation.
  • After the update, channels may no longer be available with the current configuration due to a restriction of existing approvals (F-LED is illuminated). In this case  you need to check the settings for antennas (antenna gain).
  • Because changes may occur in the national approvals while the documentation for the firmware is being completed, there may be differences between the national approvals listed in V6.2.2 and in the Compact Operating Instructions. At the time of the release, the settings according to the country list of firmware V6.2.2 are valid. There is no approval available yet for some countries. They are marked with an asterisk in the Web Based Management and Command Line Interface.

The currently available national approvals can be found in the list of wireless approvals under www.siemens.com/wireless-approvals.

 

Third-party software – license conditions and copyright notes

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the ReadMe_OSS.html file.

Special note for resellers:

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

  OSS_SCALANCE-W700_86.pdf (2.1 MB)

Description of the download procedure:

SCALANCE W780 and SCALANCE W740
For the SCALANCE W780 and SCALANCE W740 devices, you can immediately download the software as a self-extracting file "SCALANCE_W780_W740_V06_03_01.zip" free of charge. Double-clicking this file creates the following update file:

SCALANCE_W780_W740_V06_03_01.sfw

You can download the file here:

 Download unterliegt Exportcontrolle  SCALANCE_W780_W740_V06_03_01.zip (12.0 MB)
     Note: Download only for registered users

 

Then open the "System" folder in the web interface of the corresponding SCALANCE W700 product and click "Load & Save". The file "SCALANCE_W780_W740_V06_03_01.sfw" can now be imported by clicking "Load" in the "Firmware" row. Once the firmware has been successfully loaded in the SCALANCE W product, a restart is required (a browser restart is also recommended). Information on loading new firmware can be found in section 6.1 of the configuration manual: 62382125

 

SCALANCE W770, SCALANCE W760, SCALANCE W730 and SCALANCE W720
For the SCALANCE W770, SCALANCE W760, SCALANCE W730 and SCALANCE W720 devices, you can immediately download the software as a self-extracting file "SCALANCE_W770_W730_W760_W720_V06_03_01.zip" free of charge. Double-clicking this file creates the following update file:

- SCALANCE_W770_W730_W760_W720_V06_03_01.sfw

You can download the file here.

 Download unterliegt Exportcontrolle  SCALANCE_W770_W730_W760_W720_V06_03_01.zip (12.3 MB)
     Note: Download only for registered users

 

Then open the "System" folder in the web interface of the corresponding SCALANCE W700 product and click "Load & Save". The file "SCALANCE_W770_W730_W760_W720_V06_03_01.sfw" can now be imported by clicking "Load" in the "Firmware" row. Once the firmware has been successfully loaded in the SCALANCE W product, a restart is required (a browser restart is also recommended). Information on loading new firmware can be found in section 7.1 of the configuration manual: 109759652      


Download for SCALANCE W firmware version history:

You can download a version history of all firmware stages of the SCALANCE W SCALANCE W700 IEEE 802.11n as a PDF file "SCALANCE_W700_IEEE802.11n_Version_history.pdf":

You can download the file here.

  SCALANCE_Firmware_V6.3.1_DE.pdf (752.5 KB)

  SCALANCE_Firmware_V6.3.1_EN.pdf (742.4 KB)




 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.