×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109760520, Entry date: 09/11/2018
(1)
Rate

Delivery release SIMATIC Machine Simulator

  • Entry
  • Associated product(s)
Virtual commissioning saves time and money

The following is generally valid:
The later a fault is found, the more expensive his elimination. It is therefore particularly important for machine builders and plant operators to detect all faults as early as possible during the development process. Our target is to reduce the number of faults during the real commissioning phase and prevent defects.

This is enabled through virtual commissioning. The machine behavior and the control program are validated in a virtual environment. This allows to detect and eliminate all faults at an early stage already, which saves time and money.

An image of the real machine is required to perform a virtual commissioning run. This image is designated as digital twin of a machine and comprises the following three components:

  • Physical and mechanical image of the machine,

  • behavior model of the machine

  • machine automation

The following figure shows the individual components and their interaction:









Please note that the automation model of the machine can be either integrated as a real controller, or merely virtually.

The SIMATIC Machine Simulator software bundle combines the simulation software SIMIT V10 with the virtual controller SIMATIC S7-PLCSIM Advanced V2.0. This integrated software landscape for virtual commissioning provides the following benefits:
 





Available product versions:

Designation

Article number

Product description

SIMATIC Machine Simulator S V1.0

6ES7823-1HA01-0YA5

Content:

SIMIT Engineering S V10

SIMATIC S7-PLCSIM Advanced V2.0

SIMATIC Machine Simulator M V1.0

6ES7823-1HA10-0YA5

Content:

SIMIT Engineering M V10

SIMATIC S7-PLCSIM Advanced V2.0

 




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.