×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109760535, Entry date: 11/05/2018
(2)
Rate

In STEP 7 (TIA Portal) V15.1, why is it not possible to configure as isochronous centrally slotted modules in S7-1500 clock-synchronized?

  • Entry
  • Associated product(s)
After upgrading a project from STEP 7 (TIA Portal) V15 to V15.1 and updating the firmware of the S7-1500 CPU from V2.5 to V2.6, you cannot configure the centrally slotted modules as isochronous.

Description
With firmware V2.6 and higher of the S7-1500 CPUs isochronous mode is supported on the central backplane bus. The reason for the behavior described above is a non-updated module description of the centrally slotted modules. It is not enough just to update the firmware of the S7-1500 CPUs.

Remedy
Update the module description of each module. For this you open the "Properties" of the module and in the "General" tab under "Catalog information" you click the "Update module description" button.
 


Fig. 1

Then save and compile the device configuration via the menu command "Compile > Hardware (rebuild all)". You can then configure the centrally slotted modules as isochronous.

Note
You can have multiple modules of the same type upgrade synchronously.

Further Information
More information is available in the manual "SIMATIC STEP 7 Basic/Professional V15 and SIMATIC WinCC V15" under "Update Module Version".

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.