×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109760548, Entry date: 10/17/2018
(1)
Rate

SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V5.1 HF6

  • Entry
  • Associated product(s)

General information  

Attached you can find the download files of the engineering systems SIMOTION SCOUT, SCOUT Stand-alone, SCOUT TIA V5.1 HF6 and SIMOSIM V5.2 SP1 HF3.
Further information about V5.1 HF6 is available in the delivery release note 109761103 .

Four different installation packages are offered as download: 

 Installation package  Designation Directories Content
Package 1
SCOUT V5.1 + HF6
 VOL1
 SCOUT V5.1 + HF6
 (several)

 CamTool
 HSP..TM_Timer_... 
 SSP_...
 SIMOTION complete setup SCOUT V5.1 HF6

 CamTool V4.1 HFP1
 HSP for ET 200SP Timer DIDQ 
 SSPs for SINAMICS  
Installation packageDesignationDirectories Content
 Package 2
 
SCOUT Stand-alone 
 V5.1 + HF6
 VOL1
 SCOUT Stand-alone 
 V5.1 + HF6
 (several)

 CamTool
 HSP..TM_Timer_... 
 SSP_...
 SIMOTION complete setup  SCOUT Stand-alone V5.1 HF6

 CamTool V4.1 HF1
 HSP for ET 200SP Timer DIDQ
 SSPs for SINAMICS 
Installation packageDesignation Directories Content
 Package 3
 SCOUT TIA  V5.1 + HF6
(TIA Portal Client-Setup)
 VOL1 
 SCOUT TIA   V5.1+ HF6
 ScoutTia
 MigTool 
  SCOUT TIA V5.2 SP1 (incl. CamTool V4.1 HF1)
  SCOUT Migration tool plug-in V5.1 HF6

Installation package DesignationDirectories Content
 Package 4
 SIMOSIM
  V5.2+ SP1+HF3
 VOL1
 
SIMOSIM   V5.2.1.3 
 InstData 
 SIMOSIM
 V5.1 HF6
 V5.2 SP1 

 

Requirements for the installation

  • For SCOUT, SIMATIC STEP 7 V5.6 must be installed on the engineering computer.
    The SIMOTION SCOUT V5.1 HF6 is a complete installation of SCOUT.

  • For SCOUT Stand-alone, no installation of SIMATIC STEP7 V5.6 (Except an already installed SCOUT SA V5.1 HF1).

  • For SCOUT TIA, TIA Portal Framework V14 SP1 must be installed on the engineering computer (SCOUT TIA is a TIA Portal client setup). We recommend that you use the latest update of TIA Portal V14 SP1.

The shared component SIMOSIM have to be installed now via an own setup routine. Beginning from SIMOTION V5.1 HF6 and all further versions in the future of SIMOTION will not contain the SIMOSIM setup included in the frame setup of SCOUT.

 

Third-party software – Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Read_OSS file.

Special information for resellers:
The information and the license terms in the ReadMe_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing Party.

 Registrierung notwendig  Read_OSS.zip (5,8 MB)

Availability of Source Code
Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.

Siemens AG  
Digital Factory 
Customer Services DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555 
90475 Nürnberg, Deutschland 
Internet: http://www.siemens.com/automation/support-request 
Tel.: +49 911 895 7222 
Email: support.automation@siemens.com


 

Notes on the installation packages

Important notes

  • The installation packages are divided into multiple files. First download all the parts into the same folder and run the file with the .exe extension. Select the root-directory of one of your hard disks to extract the setup files. The parts are then joined up and you can execute the setup.
  • Important information:
    After starting the .exe, please ensure that the length of the selected extraction path is no longer than 32 characters. If that will be ignored, the extraction will be aborted with an error and the software can't be installed.
  • Information about SHA-256 you can find at ID 109483101

 

Installation package 1: SIMOTION SCOUT V5.1 HF6

 Registrierung notwendig  SCOUT_V5_1_0_6.exe (2,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_6.001 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_6.002 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_6.003 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_6.004 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_6.005 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_6.006 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_6.007 (610,5 MB)

 Registrierung notwendig   Registrierung notwendig  SHA-256_SCOUT_V5_1_0_6.txt (1,3 KB) (1,3 KB)



Installation package 2: SIMOTION SCOUT stand-alone V5.1 HF6

 Registrierung notwendig  SCOUT_SA_V5_1_0_6.exe (2,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.001 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.002 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.003 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.004 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.005 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.006 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.007 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.008 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_6.009 (481,5 MB)

 Registrierung notwendig  SHA-256_SCOUT_SA_V5_1_0_6.txt (1,5 KB)


Installation package 3: SIMOTION SCOUT TIA V5.1 HF6

 Registrierung notwendig  SCOUT_TIA_V5_1_0_6.exe (2,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_6.001 (667,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_6.002 (667,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_6.003 (667,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_6.004 (237,8 MB) 

 Registrierung notwendig  SHA-256_SCOUT_TIA_V5_1_0_6.txt (1 KB) 


Installation package 4: SIMOSIM V5.2 SP1 HF3

 Registrierung notwendig  SIMOSIM_V5_2_1_3.zip (55,9 MB)
SHA-256 check sum: 860BDE3BDB24942375428A9A242CC30F7B42923546E8EB409538E5DDFF8221AD


Further downloads

The following downloads are also available as a single download from the Internet Product Support pages. The components are also includes in the download of SIMOTION SCOUT and SCOUT Stand-alone (= installation package 1 and 2).

  • SIMOTION C kernel/firmware V5.1 HF1 , see 31263919 
  • SIMOTION D kernel/firmware V5.1 HF1 , see 31045047 
  • SIMOTION  Firmware Support Package (FWSP) for device update tool, see 33119786  
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.