×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109760715, Entry date: 09/19/2018
(0)
Rate

The ferrite core in the line cable for G120C FSAA 2.2kW filtered is removed

  • Entry
  • Associated product(s)
With the new design, the supplied ferrite core in the line cable is removed from G120C FSAA 2.2kW filtered variants (USS/DP/PN) supplied box.

The supplied ferrite core in the line cable is shown as item 8 in the current EMC compliant connections image.



With the new design of the filter, the ferrite in the line cable is no longer required, it will be removed from the supplied box of G120C FSAA 2.2kW filtered variants (USS/DP/PN).

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.