×
Siemens Industry Online Support
Siemens AG
文档类型 软件下载 文档编号 109760845, 文档发布日期 2020年9月9日
(37)
评估

SINAMICS Startdrive V15.1

  • 文档
  • 涉及产品
Here you can download SINAMICS Startdrive V15.1 and the corresponding updates.

Startdrive V15.1 can also be ordered directly as a DVD:

SINAMICS DCC V15.1 is available as an optional package for Startdrive Basic and Advanced V15.1 109761700

Third-party software - License terms 
You can find the copyright information for third-party software contained in this product, particularly open source software, as well as the relevant license terms of such third-party software in the following file: 

 Registrierung notwendig  Readme_OSS_All_Languages.html (2.7 MB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

OSS source code
The OSS source code files are part of the download package and can be downloaded separately here:

 Registrierung notwendig  OpenSourceSoftware.zip (2.7 MB)

Download

There is only one combined download package for Startdrive Basic V15.1 and Startdrive Advanced V15.1. Only the license key is required to use the Startdrive Advanced functionality. No further installation is required.

SINAMICS DCC V15.1 is available as an optional package for Startdrive Basic and Advanced V15.1 109761700.

SINAMICS Startdrive V15.1

Associated sales information, see 109760844 

SINAMICS Startdrive V15.1 is applicable for Startdrive Basic and Startdrive Advanced.

 Registrierung notwendig  Startdrive_V15_1.001 (2.0 GB) 

 Registrierung notwendig  Startdrive_V15_1.002 (2.0 GB) 

 Registrierung notwendig  Startdrive_V15_1.003 (515.8 MB) 

 Registrierung notwendig  Startdrive_V15_1.exe (2.8 MB)

SHA-256 checksum  Registrierung notwendig  Startdrive_V15_1.txt (1.3 KB) 

Information on the SHA-256 checksum 109483101 


SINAMICS Startdrive V15.1 Update 1

Associated sales information under 109766375 

SINAMICS Startdrive V15.1 Update 1 is applicable for Startdrive Basic and Startdrive Advanced.

SINAMICS Startdrive V15.1 Update 1 includes the complete installation of Startdrive V15.1. The installation of Startdrive V15.1 is not a precondition for SINAMICS Startdrive V15.1 Update 1.

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.001 (2.0 GB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.002 (2.0 GB) 

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.003 (518.6 MB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.exe (2.8 MB) 

SHA-256 checksum  Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.txt (1.3 KB) 

Information on the SHA-256 checksum 109483101 

SINAMICS Startdrive V15.1 Update 2

Associated sales information under 109768193 

Update 2 has been withdrawn.

SINAMICS Startdrive V15.1 Update 3

Associated sales information under 109772657 

SINAMICS Startdrive V15.1 Update 3 is applicable for Startdrive Basic and Startdrive Advanced.

SINAMICS Startdrive V15.1 Update 3 includes the complete installation of Startdrive V15.1. The installation of Startdrive V15.1 is not a precondition for SINAMICS Startdrive V15.1 Update 3.

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.001 (2.0 GB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.002 (2.0 GB) 

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.003 (520.6 MB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.exe (2.8 MB)

SHA-256 checksum  Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.txt (1.3 KB)

I
nformation about SHA-256 checksum 109483101 

SINAMICS Startdrive Basic can be used free of charge without having to enter a license key. However, for licensing reasons, you should be in possession of a SINAMICS Startdrive Basic license certificate (any version). If you do not have a license, you can order the current SINAMICS Startdrive Basic version – including the license certificate – as a DVD or you can download it. Startdrive supports the languages English, French, German, Italian, Spanish and Chinese (Simplified).

Procedure for installing Startdrive V15.1

  1. Download the attached files to a target directory on your hard disk.
  2. Please ensure that there are no spaces in the entire path name of this target directory.
  3. Start setup by calling "Startdrive_Advanced_V15_1.exe".

Eliminated functional restrictions
Detailed information on the functional restrictions which have been eliminated is provided in the lists of boundary conditions 55416849 

Data protection
Siemens observes standard data protection principles, in particular the principle of privacy by design. Further information on complying with the general data protection regulation via Startdrive   SINAMICS_Startdrive_DCC_V15_1_General_Data_Protection_Regulation_EN.pdf (96,5 KB)

Download of previous versions
Previous versions of Startdrive V15.1 can be downloaded at 109754382.


Startdrive V15.1 Support Package for SINAMICS firmware V4.7 SP13

Associated sales information under 109781776

 Registrierung notwendig  Startdrive_V15_1_HSP_FW_V4_7_SP13.zip (501.3 MB)
SHA-256 checksum  Registrierung notwendig  Startdrive_V15_1_HSP_FW_V4_7_SP13.txt (1 KB)
Information about SHA-256 checksum 109483101 
Important note: Once the Support Package is installed, it is no longer possible to upgrade the project from V15.1 to V16! Please note the following FAQs: 109782570, 109782574.
Startdrive V15.1 Update 3 is required for the installation of the Support Package for SINAMICS firmware V4.7 SP13.

Installation notes for Startdrive V15.1 Support Packages

At 54163658 you will find a description of the procedure for updating the hardware catalog of your Startdrive (TIA Portal) installation with this download.

The Support Packages can only be installed if Startdrive V15.1 update 3 has already been installed. If Startdrive V15.1 update 3 is installed again, the Support Package must also be installed again.

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。