×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109760845, Entry date: 12/13/2018
(30)
Rate

SINAMICS Startdrive V15.1

  • Entry
  • Associated product(s)
Here you can download SINAMICS Startdrive V15.1 and the corresponding updates.

Startdrive V15.1 can also be ordered directly as a DVD:

SINAMICS DCC V15.1 is available as an option package to Startdrive Basic and Advanced V15.1109761700.

Third-party software - License terms 
You can find the copyright information for third-party software contained in this product, particularly open source software, as well as the relevant license terms of such third-party software in the following file: 

 Registrierung notwendig  Readme_OSS_All_Languages.html (2.7 MB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

OSS source code
The OSS source code files are part of the download package and can be downloaded separately here:

 Registrierung notwendig  OpenSourceSoftware.zip (2.7 MB)


Download
There is only one combined download package for Startdrive Basic V15.1 and Startdrive Advanced V15.1. To use the Startdrive Advanced functionality, no further installation is required, merely the license key.

SINAMICS DCC V15.1 is available as an option package to Startdrive Basic and Advanced V15.1109761700.

 SINAMICS Startdrive V15.1

SINAMICS Startdrive V15.1

Associated sales information under 109760844 

SINAMICS Startdrive V15.1 is applicable for Startdrive Basic and Startdrive Advanced.

 Registrierung notwendig  Startdrive_V15_1.001 (2.0 GB) 

 Registrierung notwendig  Startdrive_V15_1.002 (2.0 GB) 

 Registrierung notwendig  Startdrive_V15_1.003 (515.8 MB) 

 Registrierung notwendig  Startdrive_V15_1.exe (2.8 MB)

SHA-256 checksum  Registrierung notwendig  Startdrive_V15_1.txt (1.3 KB) 

Information on the SHA-256 checksum 109483101 


SINAMICS Startdrive V15.1 Update 1

Associated sales information under 109766375 

SINAMICS Startdrive V15.1 Update 1 is applicable for Startdrive Basic and Startdrive Advanced.

SINAMICS Startdrive V15.1 Update 1 includes the complete installation of Startdrive V15.1. The installation of Startdrive V15.1 is not a precondition for SINAMICS Startdrive V15.1 Update 1.

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.001 (2.0 GB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.002 (2.0 GB) 

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.003 (518.6 MB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.exe (2.8 MB) 

SHA-256 checksum  Registrierung notwendig  Startdrive_Advanced_V15_1_UPD1.txt (1.3 KB) 

Information on the SHA-256 checksum 109483101 

SINAMICS Startdrive V15.1 Update 2

Associated sales information under 109768193 

Update 2 has been withdrawn.

SINAMICS Startdrive V15.1 Update 3

Associated sales information under 109772657 

SINAMICS Startdrive V15.1 Update 3 is applicable for Startdrive Basic and Startdrive Advanced.

SINAMICS Startdrive V15.1 Update 3 includes the complete installation of Startdrive V15.1. The installation of Startdrive V15.1 is not a precondition for SINAMICS Startdrive V15.1 Update 3.

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.001 (2,0 GB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.002 (2,0 GB) 

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.003 (520,6 MB)

 Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.exe (2,8 MB)

SHA-256 checksum  Registrierung notwendig  Startdrive_Advanced_V15_1_UPD3.txt (1,3 KB) 

Information on the SHA-256 checksum 109483101 

SINAMICS Startdrive Basic can be used free of charge without having to enter a license key. However, for licensing reasons, you should be in possession of a SINAMICS Startdrive Basic license certificate (any version). If you do not have a license, you can order the current SINAMICS Startdrive Basic version – including the license certificate – as a DVD or you can download it. Startdrive supports the languages English, French, German, Italian, Spanish and Chinese (Simplified).

Procedure for installing Startdrive V15.1

  1. Download the attached files to a target directory on your hard disk.
  2. Please ensure that there are no spaces in the entire path name of this target directory.
  3. Start Setup by calling "Startdrive_Advanced_V15_1.exe".

Eliminated functional restrictions
Detailed information on the functional restrictions which have been eliminated is provided in the lists of boundary conditions 55416849 

Data protection
Siemens observes standard data protection principles, in particular the principle of privacy by design. Further information on complying with the general data protection regulation via Startdrive

    SINAMICS_Startdrive_DCC_V15_1_Datenschutz-Grundverordnung_DE.pdf (83.9 KB)


Download of previous versions
Previous versions of Startdrive V15.1 can be downloaded at 109754382.


Notes on security
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a comprehensive, state-of-the-art industrial security concept. Siemens’ products and solutions only form one element of such a concept. You will find more information about Industrial Security at
http://www.siemens.com/industrialsecurity.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.