×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 109760897, Entry date: 09/25/2018
(0)
Rate

Firmware Update PAC2200

  • Entry
  • Associated product(s)
Update V03.00.09 (7KM2200-2EA30-1CA1, 7KM2200-2EA30-1DA1, 7KM2200-2EA30-1EA1, 7KM2200-2EA40-1CA1 7KM2200-2EA40-1DA1, 7KM2200-2EA40-1EA1)

The firmware update V03.00.09 incorporates the following modification: Small optimizations

Note!

  • This is a signed firmware package. For FW-Update, the Device must have a Version ≥ V3.0.4.
  • The use of the latest Powerconfig version is recommended.

DOWNLOAD:

 Registrierung notwendig  FW_PAC2200_V03000900_01010002.zip (301,3 KB)

Checksumme:

 Registrierung notwendig  FW_PAC2200_V03000900_01010002.fwp.txt (1 KB)
Information about SHA-256

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.