×
Siemens Industry Online Support
Siemens AG
Type de contribution : Informations sur le produit ID de la contribution : 109761027, Date de la contribution : 28/09/2018
(0)
Évaluer

Announcement of product phase-out RUGGEDCOM RSG2288 & RSG2288NC

  • Contribution
  • Concerne le/les produits(s)
The RUGGEDCOM RSG2288 and RSG2288NC will be discontinued, effective October 1, 2019. The products can be ordered using the normal process until then.

After October 1, 2019 the products will only be available as spare parts for existing customers. Repair support for these products will be provided until October 1 2028, as will support for critical security or bug fixes.


1. Discontinued products and timeline

Product name/description Article Number Phase-out announcement Product discontinuation

Product name / descriptionArticle number Phase-out announcement Product discontinuation 
 RUGGEDCOM RSG2288 6GK6022-8AS2.-.... October 1, 2018 October 1, 2019
 RUGGEDCOM RSG2288NC 6GK6022-8AS1.-....  October 1, 2018 October 1, 2019

 

2. Successor products

Depending on the requirements for the application, the following devices can be used as successors for the RSG2288/RSG2288NC;


2.1. Full gigabit 19” rack switch with IEEE 1588 Support:

The RUGGEDCOM RST2228 is the recommended successor for this use case as it is a field modular 19“ Layer 2 rack switch which supports from 4 to 24 Gigabit/s ports, up to 4 10 Gigabit/s interfaces and IEEE 1588 Transparent Clock.

More information can be found online: www.siemens.com/rst2228


Product name / descriptionArticle number 
RUGGEDCOM RST22286GK6222-6AB..-....


RUGGEDCOM products are build-to-order products. The RUGGEDCOM Selector is available for the selection and configuration of the complete order number. The RUGGEDCOM Selector can be accessed with the following URL: www.siemens.com/ruggedcom-selector


2.2. Full gigabit 19” rack switch with IEEE 1588 (Grand) Master Clock support:

The RUGGEDCOM RSG2488 is a potential successor as a field modular 19“ Layer 2 rack switch with a total of 28 x Gigabit/s interfaces and support for IEEE 1588. Besides support for transparent clock, ordinary clock, master clock the RSG2488 can be used as Grand Master Clock with the optional Precision Time Protocol Module, RUGGEDCOM RMM2431-5PTP.

More information can be found online: www.siemens.com/rsg2488

Product name / description 

Article number  
RUGGEDCOM RSG2488

6GK6024-8GS2.-....

RUGGEDCOM RSG2488NC6GK6024-8GS1.-....


RUGGEDCOM products are build-to-order products. The RUGGEDCOM Selector is available for the selection and configuration of the complete order number. The RUGGEDCOM Selector can be accessed with the following URL: www.siemens.com/ruggedcom-selector 

  
Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport