×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109761044, Entry date: 10/04/2018
(1)
Rate

Delivery release for SIMATIC CP1625 Dev (PCIe extension card for PCs) for developing a PROFINET IRT Controller.

  • Entry
  • Associated product(s)
The CP 1625 Dev is the hardware support for the development of a PROFINET IRT Controller. The CP1625 Dev can be used as PCIe extension card for PCs or stand-alone for the development of an embedded PROFINET IRT Controller. The CP1625 Dev has two Ethernet ports. The PROFINET driver must be used as controller software (to be ordered separately).
Product description:

CP1625 Dev

The CP1625  is a PCIe module for connecting PCs to PROFINET. It serves as hardware support for the development of a PROFINET IRT Controller.

  • Optimized for PROFINET IRT
  • Ethernet-Real-Time-ASIC SOC1
  • Front LEDs on the RJ45 sockets for efficient self-diagnostics of connection and data exchange (Link and Activity LED)
  • Maintenance and Error LED on the board
  • Integrated 2-port real-time switch
  • Connections
  • Two RJ45 sockets for connecting terminal devices or additional network components
  • 2 x UART interfaces
  • JTAG Debugger interface
  • PCIe interface for host operation
  • External 24 V supply for stand-alone operation (not suitable as redundant power supply in PC mode).

Areas of Application

  • Host operation: CP1625 Dev works with a host computer which is connected via PCIe. The application runs on the host computer, the PROFINET stack partly on the host, partly in CP1625 Dev.
  • Stand-alone: Application and PROFNET stack run on the CP1625 Dev

Requirements

  • Programming of the PROFINET IRT Controller using the PROFINET driver ≥ V2.1 (6ES7195-3AA00-0YA0),
    to be ordered separately 109760216 
  • Engineering of the hardware configuration in TIA Portal ≥ V15 or PNConfigLib (part of the PN driver)

Scope of delivery

 Designation DescriptionArticle number 
 CP 1625 Dev

 1 x PN IRT PCIe interface with 2 Ethernet ports, external 24V power supply, JTAG Debugger 6ES7648-2CF10-1BA0



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.