×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109761107, Entry date: 04/29/2019
(3)
Rate

Connection of an S7 1200 RTU, an S7-1500 and an ET 200SP RTU to a ST7cc central station

  • Entry
  • Associated product(s)
With the integration of the SINAUT project planning in the TIA Portal, the complete communication configuration takes place in one tool. The TeleControl portfolio has been expanded with the TIM 1531 IRC, which can be connected to the central control station as a stand-alone device. This means that one or more RTUs can be used as substations in TeleControl systems with the SINAUT ST7 protocol.

In this application example, an RTU based on SIMATIC S7-1500, a SIMATIC S7 1200 using the CP 1243-8 IRC and a SIMATIC ET 200SP using the
CP 1542SP 1 IRC are each configured in a new system with TIA Portal.

The following graphic shows the configuration scenario that is implemented in this example.



Downloads
  Documentation (2,0 MB)
 Registrierung notwendig  Project (19,5 MB)
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.