×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109761283, Entry date: 03/11/2019
(0)
Rate

How do you calculate the cycle time of the S7-1500 analog input module AI 8xU/I/R/RTD/BA according to the number and type of channels used?

  • Entry
  • Associated product(s)
The cycle time of the analog input module AI 8xU/I/R/RTD/BA of the S7-1500 (6ES7531-7QF00-0AB0) is the time interval in which the module receives new values. It depends on the type and number of activated channels.

Description
The following document shows how to calculate the cycle time for the analog input module AI 8xU/I/R/RTD/BA of the S7-1500 (6ES7531-7QF00-0AB0).

  109761283_cycle_time_analog_module_en.pdf (981,4 KB) 

Further Information
More information on the topic of Analog Value Processing, see the Entry ID 67989094.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.