×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109761403, Entry date: 10/24/2018
(2)
Rate

When changes are made in the standard user program, why do you have to load in the STOP mode with fail-safe S7-1200F/S7-1500F CPUs?

  • Entry
  • Associated product(s)
The following three scenarios describe the cause and remedy for avoiding loading in the STOP mode.

Scenario 1

Description
If you exchange data between the standard user program and the safety program, in the case of standard changes the system sometimes requires loading in STOP mode.

Example
In the safety program, read access from the standard user program to the static tag of an instance block is programmed. This data block is therefore relevant for the safety program for compiling and downloading. Now, if you change the interface of the associated function block and thus the instance block, then the safety program also has to be compiled. As a consequence, the "safety-relevant" change makes it necessary to load in STOP mode.

Remedy
For data exchange between the standard user program and the safety program we recommend that you define special data blocks (transfer data blocks) in which the data to be exchanged is stored. This decouples the blocks of the standard and safety programs. As long as these data blocks are not changed, changes in the standard program do not affect the safety program and vice versa.

Further Information
More information is available in the Programming Guideline Safety for SIMATIC S7-1200/1500 and in Section "3.9 Data exchange between standard user program and safety program".


Scenario 2

Description
If you are working on a safety program in a multiuser environment, a download in STOP might occur through the following procedure with standard changes.

Example
You make changes to the safety program in the local multiuser session. Then you load these changes directly into the controller and then synchronize the changes with the multiuser server project. You cannot mark the generated F system blocks and they are therefore not transferred into the server project.

The next time you compile and load standard changes in the multiuser server project, you have to change the F system blocks once more for the changed and this leads to loading in the STOP mode.

Remedy
Load the changes in the safety program only from the multiuser server project.


Scenario 3

Description
If you are working on a project with different STEP 7 (TIA Portal) interface languages installed on multiple PCs, project languages and when changes are made in the standard environment the system does a download in STOP with fail-safe controllers.

Example
You project has multiple project languages (German, English, for example).

  • User A has English installed as interface language and stores the project completely compiled.
  • User B has German installed as interface language.

During processing, the safety program is compiled again, without change of signature, but loading in STOP mode is necessary.

Remedy
All users must have the same TIA Portal interface languages installed. You can add more interface languages by reinstalling the TIA Portal.

Further Information
More information is available via the links in the following table:


Entry type Link 
ManualMultilingual support (S7-1500) 
Manual Basics for compiling and downloading PLC programs 
FAQIn STEP 7 (TIA Portal), why are the display texts, titles and comments no longer displayed after opening the project in the block editor? 






Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.