×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109761686, Entry date: 12/13/2018
(1)
Rate

Delivery release Target 1500S V3.0

  • Entry
  • Associated product(s)
The SIMATIC target 1500S™ for Simulink® V3.0 is now available.

Target 1500S is an add-on for Simulink from MathWorks. It enables the integration of Simulink models directly into the program cycle of an ODK-capable S7-1500 PLC.

The following new functions are available with SIMATIC Target 1500S V3.0:

  • Display of the Simulink model on the CPU web server (incl. display and changeability of model parameters and the display of signal trends in a scope)
  • Automatic transfer to the CPU: Automatic transfer of the generated SO file to  the CPU web server after each generation process directly from Simulink (including handling for access protection to the CPU with user name/password)
  • Execution of the model and reading/writing of the model parameters in different OBs possible and ensuring consistent data exchange between the call levels (thread safety)

The highlights of the other TIA Portal products can be found on the following page: 109758794

Trial-Software Download:

You can download and test a trial version of Target 1500S V3.0 for 21 days using the following entry: 109761689

Ordering data:

Please note that SIMATIC Target 1500S is only available as a software download.

DesignationArticle no.
 SIMATIC Target 1500S™ for Simulink® V3.0 6ES7823-1BE02-0YA5
 Upgrade SIMATIC Target 1500S™ for Simulink® V2.0 -> V3.0 6ES7823-1BE02-0YE5
 Target 1500S + ODK 1500S Bundle 6ES7823-1BE12-0YA0

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.