×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109761834, Entry date: 11/05/2018
(1)
Rate

Hardware Support Package “HSP0238 SIRIUS Soft Starter 3RW5 V1.0””

  • Entry
  • Associated product(s)
The Hardware Support Package „HSP0238 SIRIUS Soft Starter 3RW5 V1.0“ is available for download.

Installing the HSP0238, the hardware catalog of STEP 7 V15 can be updated with 3RW55 soft starters, the corresponding communication modules and the HMI-HF module.

The HSP is required for parameterization of the following 3RW5 modules:

  • Soft Starter 3RW55 Basic Unit V1.0
  • HMI Module High Feature V1.1
  • PROFINET Standard communication module V1.0 (Caution: To be able to use this communication module with 3RW55 the precondition is version 1.0.1)
  • PROFIBUS communication module V1.0 (Caution: To be able to use this communication module with 3RW55 the precondition is version 1.0.1)
  • Modbus TCP communication module V1.0


Requirement

The HSP0238 SIRIUS Soft Starter 3RW5 V1.0 requires the following installation:

  • STEP 7 V15 Update 3 (minimum)
  • The "HSP_V15_0238_001_Softstarter_3RW5.isp15" file must be available on the configuration PC.


Installing HSP in the TIA Portal

  1. Open the TIA Portal with administrator rights.
  2. Select "Options > Support Packages" from the menu. The "Detailed information > Installation of Support Packages" dialog box opens.
  3. Click the "Add from file system" button.
  4. Select the directory of the “HSP_V15_0238_001_Softstarter_3RW5.isp15" file in the file system.
  5. Click "Open". The file is added in the TIA Portal.
  6. Activate the "HSP0238 SIRIUS Soft Starter 3RW5" (Version 1.0) in the “Detailed information” dialog.
  7. Click the "Install" button. A dialog box opens.
  8. Close the TIA Portal.
  9. Click "Next". Installation starts.

Result

After successful installation, the "Detailed information" dialog shows the "HSP0238 SIRIUS Soft Starter 3RW5" as installed.


Download

 Registrierung notwendig  HSP_V15_0238_001_Softstarter_3RW5.zip (6,2 MB)

SHA-256 checksum:  Registrierung notwendig  Code_HSP_V15_0238_001_Softstarter_3RW5.txt (1 KB)
Information about SHA-256:  109483101 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.