×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109762326, Entry date: 07/01/2020
(1)
Rate

Delivery Release: Integration of 3VA2/3VA6 and PAC3200/PAC4200 in TIA Portal V15.1

  • Entry
  • Associated product(s)
3VA2/3VA6 and PAC3200/PAC4200 are directly supported by TIA Portal V15.1. The devices can be found in TIA Portal hardware catalog in Power supply & distribution/ Power distribution & measurement. All key parameterization and commissioning functions are available in the TIA Portal V15.1 for PAC3200, PAC4200, 3VA2 and 3VA6 with the ETUs of the 5-/8-series and all communication components.

Hardware catalog

For PAC3200, PAC4200, 3VA2 and 3VA6 with the ETUs of the 5-/8-series and all PROFINET IO and PROFIBUS DP components all key parameterization and commissioning functions are available in the TIA Portal V15.1. With integration of the devices in TIA Portal V15.1 also the integration in Energy Suite V15.1 will be supported.

TIA Portal V15.1 supports all molded case circuit frames and breaking capacity classes of 3VA2 and 3VA6 on the market.
However, consider the following restrictions when using TIA Portal V15 for EM LP products:
  • The upload of parameters of the devices to TIA Portal STEP7 V15 via SIMATIC S7 controllers is not possible. For an upload, TIA Portal must be connected to the same PROFIBUS or PROFINET as the devices.
  • The latest version of powerconfig is still necessary for a firmware update. 

At the integration of 3WLx, 3VA2/3VA6 and PAC3200/PAC4200 must be pointed out:
An upload of a SIMATIC-PLC with a connected SENTRON device is only possible if the SENTRON device has been configurated by GSD or GSDML.
Don't use the TIA Portal integrated version for SENTRON devices if the use case PLC upload.

Target market:
See target market of TIA Portal V15.1

Link:
https://support.industry.siemens.com/cs/ww/en/view/109758794


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.