×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109762788, Entry date: 12/18/2018
(0)
Rate

New features from PD LD in SIZER for Siemens Drives Version 3.19

  • Entry
  • Associated product(s)

With version V3.19 54992004, the following topics have been implemented to support PD LD business:

Highlights

SIMOTICS SD next generation (1LE5)

The SIMOTICS SD next generation motor series has been extended to include frame sizes 400 and 450.

Further, with the inclusion of SD Pro motors, for all frame sizes, it is now possible to configure the motors for line voltages higher than 480 V.

Depending on the selected power rating, the motors can be dimensioned in conjunction with the converter series SINAMICS G120P, G130, G150, G180, S150, S120 DC/AC (chassis, cabinet) – as well as S120 AC/AC converters. The load can be defined using load characteristic, simple motor selection, pump/fan/compressor and based on a mechanical system. All other selection and dimensioning steps are the same as the SIMOTICS GP/SD 1LE1 series.


SIMOTICS GP/SD VSD4000 Line

VSD4000 motors have now all been changed over to 2nd Generation versions.

This includes versions with rated speeds 3000/3600 rpm ("F" types). For these versions, SIZER now also checks the converter output frequency required.

VSD4000 motors can now be selected and dimensioned together with the following additional converters:

  • SINAMICS G120D (PM250D) with CU240D-2
  • SINAMICS G120P Chassis with PM240P-2

Additional points and updates:

SINAMICS S120 DC/AC

The portfolio has been expanded to include the following SINAMICS S120 Chassis-2 Motor Modules:

6SL3321-1TE36-6AA0

6SL3321-1TE37-4AA0

6SL3321-1TE38-1AA0

6SL3321-1TE38-8AA0


The portfolio has been expanded to include the following SINAMICS S120 Cabinet-2 Motor Modules:

6SL3721-1TE41-0BE0

6SL3721-1TE41-1BE0

6SL3721-1TE41-2BE0


The assignment of Line Connection Modules (LCM) to Line Modules (LM) has been updated for several cabinet versions.

The article numbers for Central Braking Modules have been updated.

The article numbers for Auxiliary Power Supply Modules have been updated.


1XP8 rotary pulse encoder replaced by Kübler Sendix 5020

The 1XP8 rotary pulse encoder (HTL, TTL) has been replaced by the Kübler Sendix 5020 (HTL, TTL) as the 1XP8 has been phased out.

This switchover involves the following motor series

  • SIMOTICS GP/SD 1LE1 standard motors
  • SIMOTICS GP/SD VSD10 Line
  • SIMOTICS SD 1LE5
  • SIMOTICS DP 1PC13 crane motors


SIMOTICS GP/SD VSD10 Line

VSD10 motors can now be selected and dimensioned together with the following converters, also in the voltage range 500 .. 690 V.

  • SINAMICS G120 with PM240-2
  • SINAMICS G120X
  • SINAMICS G120P with PM240P-2
  • SINAMICS G120P with PM330 (Chassis, cabinet units)

Takes into account the 30% safety margin to the stall characteristic (analogous to SIMOTICS GP/SD 1LE1).

Adaptations when assigning the speed/torque characteristics (continuous operation) based on the power classes of the motors (analogous to SIMOTICS GP/SD 1LE1).

The calculation of the motor currents for 380 V / 50 Hz and 440 V / 60 Hz has been adapted so that they correspond to the catalog values for these voltages, and no longer show what they would be like if 400 V instead of 380 V or 460 V instead of 440 V would be connected to the motor.

The NDE bearing insulation option (L51) has been approved for cast iron motors from frame size 100 and higher.

The following motor protection types have been included (15th position of the Article No.):

  • P - 1 Pt100 resistance thermometer - 2-wire connection (2 terminals)
  • Q - 3 Pt100 resistance thermometer - 3-wire connection (9 terminals)
  • R - 6 Pt100 resistance thermometer - 3-wire circuit (18 terminals)


SIMOTICS GP/SD 1LE1 standard motors

SIMOTICS GP/SD 1LE1 standard motors have been expanded to include frame sizes 63 and 71.

Winding version 2-2 is now used as standard when the following line supplies are selected:

  • 3AC 400 V, 50 Hz
  • 3AC 480 V, 60 Hz

The 87 Hz speed/torque characteristic has been adapted. The characteristic now starts approximately 3-5 % higher. This rise is compensated up to the rated speed, so that the characteristics still continue to run up to the previous torque.


SIMOTICS FD

For SIMOTICS FD motors, the calculation of the slip speeds has been corrected for versions with a rated frequency that differs from 50/60 Hz.


SINAMICS G120P Cabinet

The SINAMICS G120P cabinet series has been expanded to include the following versions with PM240P-2:

6SL3710-1PE31-5AB0

6SL3710-1PE31-8AB0

6SL3710-1PE32-1AB0

6SL3710-1PE32-5AB0


SINAMICS S120 AC/AC

The following liquid-cooled SINAMICS S120 AC/AC Chassis devices have been expanded:

Voltage 380 .. 480 V

6SL3315-1TE36-1AA7

6SL3315-1TE37-5AA7

Voltage 500 .. 690 V

6SL3315-1TG34-1AA7

6SL3315-1TG34-7AA7

6SL3315-1TG35-8AA7



Contact person

Markus Gilbert
PD LD P PPM TDM

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.