×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109762834, Entry date: 05/23/2019
(5)
Rate

How do you connect the SM 1281 to the MindSphere?

  • Entry
  • Associated product(s)
With FW3.1 MS the SM 1281 has the option of connecting directly to the MindSphere.

The document provided below describes the direct connection to the MindSphere via the SM 1281. You will receive the following information in particular:

  • Support in creating a new asset in the form of step-by-step instructions.
  • Configuration notes for the SM 1281 web page to be able to access the MindSphere.
  • List of the messages that are transferred to the MindSphere.
  • List of the ports that can be accessed with SM 1281 V3.1 MS via the Ethernet.

Download
 Registrierung notwendig  Documentation (1,5 MB)
 Download subject to export control  Firmware SM 1281 V3.1 MS (11.8 MB)
Checksum: 19E524120C3BF734F9B344EBCE2181805D59663F0E27BA8618C60796B6218FF3

Note: Delete the databases if you do a downgrade (from V3.1 MS to V3.1, for example).

Further Information
The following application example describes how to connect to the MindSphere with the MindConnect Nano: 109750010 

Additional Keywords
Asset, Mind-Sphere, SM1281, CMS, Asset Manager, Assetmanager, MindConnectLib, MindConnect-Lib, MindConnect, CMS1200, SIPLUS, connectivity


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.