×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109763136, Entry date: 03/18/2019
(4)
Rate

Siemens Network Planner – Download SINETPLAN V2.0 Trial

  • Entry
  • Associated product(s)
The trial version for SINETPLAN V2.0 is now available for download. The Siemens Network Planner supports planners of automation systems based on PROFINET and supports the professional and proactive simulation of the network of a system.


Download:  Trial Version SINETPLAN V2.0

As a registered customer, you can download the trial version for SINETPLAN V2.0.

The new features are described in the delivery release for SINETPLAN V2.0.   109763494



This download offers the following options:

  • Trial Version SINETPLAN V2.0  (for new customers,  test version for 21 days)
The trial version does not support import and export functions or Pcap analysis.
An example project for testing can be found under the following entry:  109743227


  • NOTICE:
This trail version is intended for testing purposes only.
It may not be used to update an installed SINETPLAN version.
Your installed SINETPLAN version may become unusable by updating to SINETPLAN V2.0.
A successful update to version V2.0 requires a SINETPLAN V2.0 license.




Notes about downloading
The software is subjected to export restrictions. Download is only possible for registered users. Please note that, on account of the strong demand, the registration for export-restricted downloads will take some time.


SHA-256 checksum (Information on SHA-256)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit