×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109763251, Entry date: 01/29/2019
(2)
Rate

Local Download Software Controller

  • Entry
  • Associated product(s)
Download a TIA Portal project locally into a SIMATIC S7-1500 software controller without engineering laptop.

This document shows you how to load a TIA portal project locally into a SIMATIC S7-1500 software controller. In this case, both the Engineering SIMATIC STEP 7 TIA Portal and the SIMATIC S7-1500 Software Controller are installed on the same SIMATIC IPC.
Engineering and control are installed on the SIMATIC IPC 427E. The download of the TIA Portal project into the software controller is done via an internal SIMATIC Communication.


Hardwareaufbau des Simatic IPC

This allows you to dispense with an additional engineering notebook during engineering.

Download
  109763251_SWControllerLokalerDownload_DOC_V10_en.pdf (847,7 KB)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.