×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109763254, Entry date: 02/14/2019
(1)
Rate

Connection between software controller and WinCC V7 via Windows network

  • Entry
  • Associated product(s)
Establish an HMI connection between a SIMATIC S7-1500 Software Controller and SIMATIC WinCC V7.4 SP1.

This document shows you how to establish an HMI connection between a SIMATIC S7-1500 Software Controller and SIMATIC WinCC V7.4 SP1 via the Windows network.
In the software CPU 1507S variables are made available in a global data block for the visualization software SIMATIC WinCC V7.4 SP1. The visualization computer does not have to be located in the PROFINET network, since a communication connection can be established via the virtual interface (V2 and V1) of the software controller (V2.5) with IP routing. Thus, the visualization computer can also be physically located in the Windows network and connected to the software controller computer via the Windows interface (X1).


Hardwareaufbau der beiden SIMATIC IPCs

Download
  109763254_SWControllerWinCCExtern_DOC_V10_en.pdf (2,0 MB)

For further information go to
Joint Operation of WinCC V7 or WinCC V14/15 RT Prof. and Software Controller

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.